STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

CubeMX bug report: error in generating stm32f4xx_it.c

Posted on August 02, 2016 at 18:01Hi,If in NVIC Configuration -> Code Generation, none of the IRQ handlers are selected, the generated stm32f4xx_it.c file is not generated, but reads a java backtrace:/* Includes -------------------------------------...

Resolved! Selecting 8MHz clock on Nucleo-64 in STM32CubeMX

Posted on January 04, 2017 at 07:53I'd like to migrate a project from using the internal RC on the STM32F091RC to the 8MHz HSE clock that comes down from the on-board ST-LINKV2's MCO signal.  I use STM32CubeMX to generate SystemClock_Config().  On t...

STM32 Cube

Posted on January 03, 2017 at 15:24Under Project > Settings Advanced Settings in the Drive Selector section for IP Name I see SPI, USART, etc. Under Driver the choice is HAL and cannot be changed. How does one change that selection to another choice...

John Hite by Associate III
  • 3629 Views
  • 9 replies
  • 0 kudos

Resolved! Cube MX and VECT_TAB_OFFSET

Posted on October 05, 2016 at 17:48Hello,i am using a custom made bootloader on an stm32f107. So i need to change VECT_TAB_OFFSET in the application code to offset the vector table. But every time when i`m generating code with Cube Mx the file syste...

tekampe by Associate II
  • 4337 Views
  • 5 replies
  • 0 kudos

cubeMX stm32f042 custom HID USB problem

Posted on December 23, 2016 at 03:36Hello everyone! I use CubeMX to generate projects for stm32f042f6 USB custom HID mode,  when I configured parameters ,download to my circuit board,connect it to PC,but the USB HID Demonstrator do not display any m...

0690X00000605tgQAA.png 0690X00000605vzQAA.png 0690X00000605wTQAQ.png 0690X00000605wYQAQ.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.