STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

stm32cube lwip clean code but no link?

Posted on December 08, 2016 at 12:31hi everyone. im new at stm32 and im trying to use lwip with cubemx (firmware :stm32cubef4  v1.14.0). my board is stm3241g-eval. and i investigated example projects and it works (ex. udp echo client) I created a ne...

STM32CubeMX 4.18.0 - bug, deleted startup_stm32fxxxxx.s

Posted on November 27, 2016 at 02:16I tried the new version of STM32CubeMX 4.18.0. If I generate project for MDK-ARM V5 will be deleted the startup_stm32fxxxxx.s file in the path Drivers/CMSIS/Device/ST/STM32Fxxx/Source/Templates/gcc. Similarly, if...

CubeMX 4.18.0 compatible processor conversion bug

Posted on November 28, 2016 at 23:27I converted my project from using a '407VGT6 to using a '405VGT6 (very painless), BUT I lost all of my DMA settings and all of my interrupt priorities.Version control is my friend.Andrei from The Great White North...

STM32 Nucleo L476 Internal Temperature Sensor

Posted on July 20, 2016 at 23:00Hello,I'm trying to get the internal temperature sensor to work. But the whole time, the sampled values are too low. If I use that fancy formula from the reference guide, it says there are about 10�C, but believe me, ...

STM32L4 without Crystal for CAN, I2C and SPI

Posted on November 15, 2016 at 11:00Hello everyone,I am planing a few Sensors and remote switches which communicate using the CAN Bus. I'd like to use the STM32L433CC MCU because of its easy solderability by hand for prototyping. The boards should b...

STM32CubeFx Examples generated by STM32CubeMX

Posted on February 26, 2016 at 10:34Hi CubeMX team, why are not firmware examples for development boards written using STM32CubeMX ? I think it would help to quickly find errors in STM32CubeMX. Also, customers should share original ioc file for dev...

CubeMx 4.17 does not handle -q or -s switch

Posted on November 28, 2016 at 15:38 Hi, I recently discovered in UM1718 that CubeMX can work with a command line. That's a cool feature for continuous integration. But it seems that the command line switch are not handled. If I use ...

JulienD by Senior
  • 3208 Views
  • 7 replies
  • 0 kudos

Bug, Code generation in STM32CubeMX

Posted on September 26, 2016 at 07:16Hello,I used STM32CubeMX with 4.16.0 or 4.16.1 version.below situation :''STM32Cube Firmware Library Package'' option is ''Add necessary library files as reference in the toolchain project configuration file''IAR...

0690X00000604maQAA.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.