STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1759 Views
  • 0 replies
  • 2 kudos

STM32F407 + UDP+LWIP big packet problem

Posted on August 16, 2017 at 00:58Dear Forum,I bring forth a frustration question yet I'm uncertain how to approach it.I have STM32F402, and I can communication over UDP . In cube I reviewed every options but my problem do not solved. If I can sendi...

lorant124 by Associate III
  • 1415 Views
  • 1 replies
  • 0 kudos

Resolved! Upgrade of lwIP embedded in STM32CubeMX

Posted on December 14, 2016 at 12:11Hello ST,I'd like to ask if there are plans to upgrade the lwIP embedded (1.5) in the Cube to the recent release 2.0.0Meanwhile, I can assure that upgrading an existing Cube project is possible!If someone is inter...

infor by Associate III
  • 3096 Views
  • 5 replies
  • 0 kudos

EEPROM for Cube MX STM32F301C8

Posted on August 07, 2017 at 09:13Hi,I would like to used EEPROM for STM32F301C8. I am used code belowuint32_t READ_FLASH(uint32_tDataAdr){ return *(int32u *)DataAdr;}void WRITE_FLASH(uint32_tDataAdr, uint32_tData){ erase_pages.PageAddress=DataAdr; ...

Gz by Senior
  • 2587 Views
  • 6 replies
  • 0 kudos

STM32F767 SRAM problem

Posted on July 28, 2017 at 09:25Hello, i made my own devkits with huge altera and STM32F4/7 micro-controllers.As usual, STM32F479 performing very well, it uses 26b ADR, 32b data lines directly to FPGA.But for some reason code generated by STM32CubeM...

Resolved! CubeMX generates wrong I2S frequency on STM32F401C-Discovery

Posted on August 02, 2017 at 11:42I have a clean slate CubeMX project on a STM32F401C-Discovery board. I have set up the onboard Cirrus audio DAC, and send a hard-coded test signal to it via DMA-driven I2S. I can hear the sound, but it is at wrong f...

0690X00000607mlQAA.png 0690X00000607ptQAA.png 0690X00000607pyQAA.png
kraiskil by Associate III
  • 8439 Views
  • 14 replies
  • 0 kudos

Resolved! Possible HAL F429 UART TX Bug

Posted on July 31, 2017 at 13:36Hi, I am working on my project which requires to send some data over UART.I have F429ZI Nucleo board with a UART2 configured (see uart2_config image). The UART2 has Interrupts enabled so I can use the HAL_UART_Transmi...

dman by Associate II
  • 10885 Views
  • 12 replies
  • 0 kudos

Resolved! CubeMX 32-bit SDRAM with STM32F469IIT

Posted on July 31, 2017 at 23:37I'm using CubeMX with the STM32F469IIT and trying to select 32-bit wide SDRAM using the FMC but the options only show 8 or 16-bit.Is this correct? I can't see anything in the reference manual about the LQFP176 not bei...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.