STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

MX_TIM2_Init() hangs debugging

Posted on September 18, 2017 at 13:25 Hi, I use Stm32CubeMX v4. It creates the code for TIM2, TIM3 and TIM8 (STM32F103VCT, custom board). All timers have 'Clock Source == Internal Clock' and 4 channels configured to 'Input Capture direct mode'. W...

Boris Hoz by Associate II
  • 4663 Views
  • 8 replies
  • 0 kudos

Cube MX missed or incomplete FATFS support

Posted on August 11, 2017 at 18:39Hi Everyone, recently I am trying uSdCard FATFS library configured and generated from cubemx tool(v4.22.0),Only when I enable _USE_LFN parameter which is for long file name support I received compilation errors, Bel...

Resolved! STM32CubeMX USB control request

Posted on September 11, 2017 at 21:16 Hi there, I am using STM32CubeMX to develop a USB HID touchscreen with the STM32F103C8T6 MCU. In the HID descriptor, I must report the following feature to support multi-touch: 0x85, REPORTID_MAX_CO...

Ted NIVAN by Associate II
  • 2733 Views
  • 4 replies
  • 0 kudos

Resolved! [CubeMX regression]Failed to generate code with 4.22.1

Posted on September 13, 2017 at 08:46The new CubeMX 4.22.1 fails to generate code (and hangs on generation) for a STM32 workbench project which has been successfully generated with the previous versions.Here is the command line output from the probl...

I can not get atr by using of st's code

Posted on September 12, 2017 at 14:11Hi, I am new to stm and I have STM32L053R8 - NUCLEO, I have to make a smartcard project with this.I am using prepared code by given ST Firm and a smartcard. When I debug the code , it stucks. the code of smartcar...

STM32F207 cubeMx CAN problem

Posted on August 25, 2017 at 09:01Hi,I recently started programming on the STM32F207 nucleo board and I ran into a problem.I used CubeMx to create initialisation code for CAN1 and it doesn't seem to work.I'm trying to implement CAN with interrupt. B...

''C'' STM32 ADC Project to ''Cpp'' (CubeMX)

Posted on September 12, 2017 at 10:32 Hi everyone, I'm trying to convert a 'C' generated project with CubeMX in 'Cpp' but I have some problems with that. Indeed with CubeMX I have generate a project to read ADC values. This one work fine. The sam...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.