2017-07-14 2:56 PM
ccsbcs.c of FatFS 3rd Party Lib is not copied from CubeMX repository to projects folder which prevents a compilation of the created project. Copying this file manually fixes compilation errors which give misleading messages.
I found this with SW4STM32 + CubeMX 4.22 + STM32F429ZIT + SDIO on Win7.
Best regards,
Markus.
#stm32f429 #cubemx #fatfs-sdioSolved! Go to Solution.
2017-09-18 3:33 AM
Hi Markus
A fix was delivered in the CubeMx 4.22.1 version (released a few days ago).
Using it you will be able to verify if the issue you reported us was finally solved.
Regards,
Fred
2017-07-15 3:02 PM
Hello
Horbach.Markus
,I will check this issue and report it internally if confirmed.
We will come back to you when we have update.
Regards
Imen
2017-08-09 8:53 AM
For information, a fix is being implemented, and, if the first (positive) tests are confirmed during the validation phase, it should be available in the next official Mx version.
Furthermore, the issue seems to be linked to the USE_LFN value (not a surprise): with the default value (disabled) in Mx, I cannot reproduce the issue. When it is enabled, the issue is reproduced for SW4STM32 (while it seems ok with IAR and Keil).
Regards
Fred
2017-09-18 3:33 AM
Hi Markus
A fix was delivered in the CubeMx 4.22.1 version (released a few days ago).
Using it you will be able to verify if the issue you reported us was finally solved.
Regards,
Fred
2017-09-19 6:33 AM
Hello Fred,
I checked CubeMX4.22.1 with STM32F429i-Disco and STM32F746G-Disco and now FATFS works fine,
the formerly missing file is now copied to the Project.
THX.
Best regards,
Markus.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.