STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Resolved! Bug report: STM32CubeMX 4.23 MX_RTC_Init

Posted on October 26, 2017 at 10:35Today I have just updated my STM32CubeMX to the 4.23 version.I migrated the project I am using currently. It uses a STM32F767VITx. So far, I was using the 4.21.1 version of STM32CubeMX.Today I made some changes in ...

0690X00000608lEQAQ.png

Resolved! Bug when creating STM32L4 based projects using CubeMX

Posted on July 21, 2017 at 11:02I am trying to create a project for either the L469 Discovery or Nucleo-144 board using CubeMX.My setup is the following:CubeMX 4.22.0L4 Firmware v1.8.1Using STM32 AC6 latest versionIt appears as though CubeMX does no...

Ant M by Associate II
  • 2626 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F746 CubeMX clock not reporting correctly?

Posted on October 25, 2017 at 18:38I'm using an STM32F746VGT6 microcontroller configured from STM32CubeMX for all the clocks and I'm getting roughly 220% higher clock rates reported for SystemCoreClock when compiled. For instance I have an HSE cryst...

0690X00000608kWQAQ.png

Resolved! STM32CubeMX display resolution problem

Posted on June 27, 2017 at 16:27Hello ST team,I think the STM32CubeMX code generator has a big problem with screen resolution. I'm using a laptop with 4K display, so my CubeMX appears like following screenshots, which are annoying in many cases: Alm...

0690X00000607RtQAI.png 0690X00000607UdQAI.png
misagh by Associate III
  • 6327 Views
  • 13 replies
  • 1 kudos

I found a Bug about the NAND Flash Driver of STM32F7

Posted on October 24, 2017 at 06:21When I meet a bad block in a NAND flash,it will stop here forever.The 'tickstart = HAL_GetTick()' should put in front of 'while(HAL_NAND_Read_Status(hnand) != NAND_READY)'.#nand-flash-driver #stm32cubemx #bug

0690X000006049kQAA.jpg

stm32cubeMX doesn't modify/generate the system_stm32l0xx.c

Posted on October 17, 2017 at 12:49Hi All,in order to build new project (using STM32l073v8t processor) folder, I used the STM32cubeMX.I've set all IOs, change the clock tree using its UI and etc' according to my project.When I check the generated co...

moranf by Associate II
  • 1983 Views
  • 3 replies
  • 0 kudos

STM32CubeMX LL Driver Issues

Posted on July 25, 2017 at 11:08I found two issues with the latest (and updated) STM32CubeMX when generating a Makefile project for STM32F334 Nucleo64 board.1. I selected only the LL drivers but the Makefile had the 'USE_HAL_DRIVER' definition, so t...

Resolved! STM32L452CEU6 HSI Problem

Posted on June 03, 2017 at 20:12I have a board which was designed to use the STM32L433CCU6 and am attempting to use it with an STM32L452CEU6.  The board works perfectly fine with the 433, but I am struggling a bit with the 452.  The problem I was fa...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.