STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1759 Views
  • 0 replies
  • 2 kudos

Error[Lp050] in AWS CubeMX expansion

Posted on September 07, 2017 at 18:31I am trying to compile the CubeMX expansion for AWS, but I get an Error[Lp050]: placement includes both uninitialized sections (example 'ro data section UNINIT_FIXED_LOC in iot_flash_config.o symbols: [lUserConfi...

USB composite device first packet always empty

Posted on November 13, 2017 at 23:41Hi,I am working with STM32F072RB and I am developing composite device. The device consists of 3 different interfaces but only one has in and out endpoints. It's custom HID with input and output report of 64 bytes....

Nix Wayne by Associate III
  • 1562 Views
  • 2 replies
  • 0 kudos

Issue with STM32F7 SPI interface

Posted on November 10, 2017 at 08:05I am using the STM32F765BIT micro controller(208 pin package) in our custom board, I am using STM CubeMx generated code. I have selected two SPI (SPI1 & SPI2) interface both are with same configuration. with SPI2 ...

MANISH by Associate II
  • 912 Views
  • 1 replies
  • 0 kudos

Resolved! power consumption calculator for stm32h7

Posted on October 17, 2017 at 22:27Hello,I am trying to estimate power consumption on the stm32h7. The use case i am interested in is sampling 6 channels using ADC3 and transferring the sampled data to memory using BDMA, all this while D1 and D2 dom...

STMCubeMX repository folder

Posted on October 10, 2017 at 23:15I know it's kind of stupid. But I still want to make sure if the repository folder can be changed? Because the capacity of my C is not big enough.#stmcubemx

Simulink model sample time vs. STM32 MCU clock configuration

Posted on November 07, 2017 at 12:53Hello everyone, In this project I just want to use the user button to toggle a LED on my board. The model is designed by using Simulink and initialization codes are generated by STM32CubeMX. During the experiment...

0690X00000608rqQAA.png 0690X00000608sFQAQ.png
Sam Q. by Associate III
  • 2332 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F407G-DISC1 : not listed in STM32CubeMX

Posted on November 02, 2017 at 14:15Hello,I'm new to this exiting world of MCUs.I tried many installs from scratch, did all the available updates I found, but I still can't see my 'STM32F407G-DISC1' in the list of boards in STM32CubeMX.I find 2 'STM...

Resolved! MCU initialization fail while using HSE?

Posted on November 02, 2017 at 18:18I am using NUCLEO-F767ZI board where I observe that when I use the internal clock (HSI), the mcu runs fine, but when I configure the cubeMX project to run on external 8MHz clock (HSE), the mcu fails to run. Follow...

0690X00000608o4QAA.png 0690X00000608ikQAA.png

FLASH_WaitForLastOperation CubeMx error

Posted on January 23, 2017 at 10:02The latest Version of CubeMx (4.19.0) the 'FLASH_WaitForLastOperation' function causes errors if the HAL_GetTick() function is near its rollover point. The cause seems to be 'uint32_t timeout = HAL_GetTick() + Time...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.