2016-06-08 7:48 AM
Hi,
setting the ADC1_IN8 or ADC_IN15 as OPAMP x Output Differential or OPAMP x Output Single-ended in STM32CubeMx v 4.15 with NUCLEO-L476RG doesn't generate the correct GPIO setup. The OPAMP output pins are configured as GPIO_MODE_ANALOG under HAL_OPAMP_MspInit in stm32l4xx_hal_msp.c while they should be configured as GPIO_MODE_ANALOG_ADC_CONTROL to feed the ADC. There is also another error: setting the the ADC1_IN8 or ADC_IN15 as OPAMP x Output Differential generates the wrong regular channel configuration as ADC_SINGLE_ENDED. It should be ADC_DIFFERENTIAL_ENDED. Regards #stm32-cubemx-opamp-adc2016-06-09 1:45 AM
Hi dallagiovanna.luca,
Thnak you for the feedback. I report this internally to our CubeMx team. -Hannibal-2016-12-28 4:59 AM
Hi!
In CubeMX v.4.18.0 this problem present.
The OPAMP output pins are configured as GPIO_MODE_ANALOG under HAL_OPAMP_MspInit in stm32l4xx_hal_msp.c while they should be configured as
GPIO_MODE_ANALOG_ADC_CONTROL to feed the ADC.2017-07-06 12:28 AM
Hi,
the GPIO_MODE_ANALOG / GPIO_MODE_ANALOG_ADC_CONTROL Bug was reported in June, 2016, one Year ago.
Now, in CubeMX 4.21.0 with firmware V1.8.1 it still exists. Is there a chance that this will be fixed?
2018-01-18 4:55 AM
Hi
Dallagiovanna.Luca
andZottmann.Nils
,Sorry for the late answer.
I confirm that the 2 points
Dallagiovanna.Luca
you highlighted are taken into account by the development team.I can't give you any delivery date butI will keep you inform as soon as both corrections are integrated in a new CubeMX release.
BR. Jeanne
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.