STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1755 Views
  • 0 replies
  • 2 kudos

CubeMX FREERTOS CMSIS_V2 LWIP - RTOS Dependency

Hello, what do I wrong?  I am trying to setup a new stm32f7xx project, with CMSIS_V2 and LWIP.I use only the CubeMX application at the version 6.15.0, I have tried several hours to get this setting but nothing working.If I select CMSIS_V1 the LWIP us...

Joe94_0-1753131317903.png Joe94_1-1753131376550.png Joe94_2-1753131549084.png
Joe94 by Associate II
  • 1359 Views
  • 5 replies
  • 1 kudos

bug in FMC configuration of SDRAM in CubeMX 6.14

16bit SDRAM with 4 banks, 9bit column address, 13bit row should show as 32MB memory area,but it is shown as 16MB.You have to change column address bits to 10bit and back to 9 bits to set the value correctly (32MB).It is dangerous beacause code genera...

trzeci by Associate III
  • 1492 Views
  • 4 replies
  • 1 kudos

error:"This feature requires internet connection"

  When I try to log in to my ST account in STM32CubeMX, it sends me an error message that says, 'This feature requires an internet connection.' However, my internet connection is working well, and I can use other browsers to surf the internet normall...

屏幕截图 2024-07-13 134732.png
Pea by Associate
  • 2891 Views
  • 3 replies
  • 0 kudos

STM32CubeMX 6.15.0 issue

I just updated CubeMX to 6.15.0 and I can't start a new project anymore.The spinning wheel keeps sinning forever after going File/New Project or clicking on any on the shortcuts on the right side of the screen under "I need to:" section.I tried to re...

vard by Associate II
  • 711 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.