STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Bug Report: CubeMX Generates Bad Init Code

Posted on March 17, 2018 at 21:08 Like • Show 0 Likeshttps://community.st.com/0D50X00009Xkg1FSAR Comment • https://community.st.com/0D50X00009Xkg1FSAR&sharpcommentsUsing CubeMX V4.7.25.0 I get initialization code for RTC.c that won't compile wh...

STM32L4 DISCO USB DEVICE DOES NOT WORK

Posted on April 11, 2016 at 11:19I used CUBEMX (Version 4.14.0) to generate a small usb test program for stm32l4 discovery board. The L4 Lib is Version 1.4.0. When i only initialize USB as device (class CDC) it doesnt' work. All registers seem to b...

Leo_Panda by Associate III
  • 3160 Views
  • 7 replies
  • 0 kudos

CubeMX makefile issue + makefile template

Posted on May 30, 2017 at 08:55Hi guys,CubeMX supports makefile generation starting from 4.21.0 version. I've tested the makefile, however, there are some issues:Major issues:- missing header files dependency (make won't update the output in case a ...

bug in stm32cubemx 4.23 makefile generator

Posted on November 19, 2017 at 21:26(I'm sorry if this is the wrong place to report this)STM32CubeMX 4.23 (tested with MacOS High Sierra, Arch Linux x86_64 with x32 binary emulation) is generating spurious entries during Makefile generation (such as...

CubeMX adc rank number bug

Posted on May 30, 2018 at 14:33Hello there,When configuring an ADC periph (STM32L452) the ranks are assigned incorrectly. Cube generates this:sConfig.Rank = 1;sConfig.Rank = 2;// etcInstead of this:sConfig.Rank = ADC_REGULAR_RANK_1;sConfig.Rank = AD...

0690X0000060BS0QAM.png

about STM32CubeMx question

Posted on June 01, 2018 at 05:35STM32CubeMX generate code in keil5 ,when project into debug environment ,why no periphral register window?#stm32cubeprogrammer

ann Qian by Associate
  • 957 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubxMX software

Posted on June 01, 2018 at 05:43what the advantage and convienient of STM32CubxMX  generate Code in keil5 compare to classic library? Is there some documents for user about STM32CubxMX  generate Code ? The principle of STM32CubxMX  generate Code is ...

ann Qian by Associate
  • 1103 Views
  • 1 replies
  • 0 kudos

USB CDC breaks on heavy load

Posted on May 30, 2017 at 19:08Hi,I'm currently evaluating the STM32F072 Discovery. We are tending moving from ATXMega to ARM and I have to verify if the device is fitting our needs, before investing more time in learning a new architecture.I succes...

Klaus U by Associate
  • 3082 Views
  • 3 replies
  • 0 kudos

STM32H743 TIM2 input compare

Posted on May 19, 2018 at 10:48Hi,I can not get the input compare mode working as expected. I need to use TIM2 CH1 as trigger to measure the frequency of external pulses. I have used the methode on a STM32F091 where it works fine.RCC and GPIO are in...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.