STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

CubeMX New project trouble empty,blank and white window

I have same trouble with this link --> https://community.st.com/s/question/0D50X00009XkYPHSA3/stm32cubemx-blank-new-project-page?t=1543518688382I have trouble with cubeMX when i try to create new project cannot see anything only white,blank and emty ...

akos by Associate II
  • 1686 Views
  • 2 replies
  • 1 kudos

I need an example or description of how to define the function parameter device pObj that appears in all the ENV sensor function calls in the STM32Cube.

I started out with an example bare-metal project for the B-L475W-IOT1A Discovery board, that reads the HTS221 temperature and humidity, and LPS22HB pressure. Very straight forward. For ex, api to read temp: float HTS221_T_ReadTemp(uint16_t DeviceAddr...

eskul by Associate
  • 1150 Views
  • 0 replies
  • 1 kudos

bugreport: CRC on STM32L011D4 (CubeMX5.0.0)

Generated code not contains hcrc declaration.MX_CRC_Init func is empty (contains only comments)Сonditions:STM32L011D4 is used as mcucrc module in enabled in cube mxp.s.Please make version 4.x available for download from the site as an option.Forced b...

F303RE Nucleo analogue reading inconsistency

Pretty much the code is generated by Cube.I am reading 11 adc's some on adc1 and some on adc2. If I put the pins to 0 gnd i have consistent reading 0. All pins to 3.3v I have But reading in a looppa7,pa7,pa7,pa7,pa7,pa7pa7 4095pa7 4095pa7 4031pa7 403...

Marius CO by Associate III
  • 921 Views
  • 0 replies
  • 0 kudos

use fifo checkbox

There used to be a checkbox "use fifo" where i could chose duble buffer dma, but now there is no such function. (see screenshot) Why? Can anybody say me please, you havent this too?PS: New CubeMX 5.0.0 design is so terrible ((

mkozi.17 by Associate II
  • 1471 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.