2018-11-29 2:28 PM
Pretty much the code is generated by Cube.
I am reading 11 adc's some on adc1 and some on adc2. If I put the pins to 0 gnd i have consistent reading 0. All pins to 3.3v I have
But reading in a loop
pa7,pa7,pa7,pa7,pa7,pa7
pa7 4095
pa7 4095
pa7 4031
pa7 4031
pa7 4032
the value varied from 4032 to 4095
Now in a 3.3v/2 divisor varies from 1965 to 1929
pa7 1929
pa7 1929
pa7 1930
pa7 1950
pa7 1965
pa7 1964
pa7 1965
then all pins to 0
pa7 0 for gnd
pa1 0
pa0 0
pa5 0
pa6 0
pc0 0
pc1 0
pc2 0
pc3 0
3.3v all pins reads different values
pa7 4028 for 3.3v
pa1 4020
pa0 4017
pa5 4032
pa6 4026
pc0 4020
pc1 4013
pc2 4018
pc3 4017
I have a termistor and calc formula gives temp errors in orders of 10 degress
My adc init is for both adc's:
static void myInit_Adc(ADC_HandleTypeDef* hadc)
{
hadc->Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
hadc->Init.Resolution = ADC_RESOLUTION_12B;
hadc->Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc->Init.ScanConvMode = ADC_SCAN_DISABLE;
hadc->Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc->Init.LowPowerAutoWait = DISABLE;
//hadc->Init.LowPowerAutoPowerOff = DISABLE;
hadc->Init.ContinuousConvMode = DISABLE;
hadc->Init.DiscontinuousConvMode = DISABLE;
hadc->Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc->Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc->Init.DMAContinuousRequests = DISABLE;
hadc->Init.Overrun = ADC_OVR_DATA_PRESERVED;
}My channel config is:
tatic void myInitChannels(ADC_HandleTypeDef* hadc,
ADC_ChannelConfTypeDef* sConfig)
{
uint32_t channels[]={ADC_CHANNEL_1,
ADC_CHANNEL_2,
ADC_CHANNEL_3,
ADC_CHANNEL_4,
ADC_CHANNEL_5,
ADC_CHANNEL_6,
ADC_CHANNEL_7,
ADC_CHANNEL_8,
ADC_CHANNEL_9,
};
uint32_t ranks[]= {ADC_REGULAR_RANK_1,
ADC_REGULAR_RANK_1,
ADC_REGULAR_RANK_1,
ADC_REGULAR_RANK_1,
ADC_REGULAR_RANK_1,
ADC_REGULAR_RANK_1,
ADC_REGULAR_RANK_1,
ADC_REGULAR_RANK_1,
ADC_REGULAR_RANK_1,
};
for(int c=0; c<sizeof(channels)/sizeof(channels[0]);c++)
{
sConfig->Channel = channels[c];
sConfig->Rank = ranks[c];
sConfig->SingleDiff = ADC_SINGLE_ENDED;
sConfig->SamplingTime = ADC_SAMPLETIME_61CYCLES_5;//ADC_SAMPLETIME_1CYCLE_5;
sConfig->OffsetNumber = ADC_OFFSET_NONE;
sConfig->Offset = 0;
if (HAL_ADC_ConfigChannel(hadc, sConfig) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
}
}My select channel function is
void select_adc(uint32_t channel, ADC_HandleTypeDef* ahd, bool sel)
{
ADC_ChannelConfTypeDef sConfig;
if(sel)
{
sConfig.Channel = channel;//ADC_CHANNEL_1;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SingleDiff = ADC_SINGLE_ENDED;
sConfig.SamplingTime = ADC_SAMPLETIME_61CYCLES_5;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(ahd, &sConfig) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
}
else
{
sConfig.Rank = ADC_RANK_NONE;
if (HAL_ADC_ConfigChannel(ahd, &sConfig) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
}
}My analogue read is:
static void _anal_read(struct AnalogPin* pin)
{
int32_t values[4];
bool err=false;
if(pin->fromIT)
{
if(pin->calcFoo)
{
(*pin->calcFoo)(pin);
}
return;
}
select_adc(pin->channel,pin->adc,true); //channel
for(int i=0;i<4;i++)
{
if(HAL_OK==HAL_ADC_Start(pin->adc))
{
if(HAL_ADC_PollForConversion(pin->adc, 1000) == HAL_OK)
{
values[i] = HAL_ADC_GetValue(pin->adc);
}
else
{
if(ERRREPO)
{
printf("# ? Error adc pool\r\n");
err=true;
break;
}
}
while(HAL_OK!=HAL_ADC_Stop(pin->adc))
{
;
}
HAL_Delay(8);
}
}
if(!err)
{
select_adc(pin->channel,pin->adc,false); //channel
pin->curval = (values[1]+values[2]+values[3])/3;
if(pin->calcFoo)
{
(*pin->calcFoo)(pin);
}
return;
}
pin->curval = -1;
if(ERRREPO)
printf("# ? ADC failed this time\r\n");
}Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.