STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

STM32CubeMX - Conflicting Generated Function Call Ranks

I have a fairly simple project defined in CubeMX based on one of the H7-series of STM32 parts. This project utilizes a number of peripherals and DMA channels, including the MDMA and RTC peripherals.As I configured an additional DMA channel for a USA...

BHans by Associate
  • 2663 Views
  • 5 replies
  • 0 kudos

ADC DMA Callback Stops after Running Once

The base software was set up using CubeMX. On an STM32L433, I have the ADC configured to read 4 channels into a DMA. The sampling is ADC_SAMPLETIME_6CYCLES_5 for all channels. The DMA is set up for a WORD transfer into a buffer: uint32_t dmaBuffer[4...

code generation is hanging because of cloud station backup

Hi everyone,On my system, there is cloud station backup working in background, so each file that is modified is back-up on distant synology server.This works very fine...Problem is, if starting code generation of STM32CubeMX, code generation starts a...

Resolved! Unable To Select ADC->ScanConvMode on Device

Hello:I am using the STM32L433 device.In CubeMX, I am using ADC1 channels 5,6,9 and 15. Other than the yellow highlights, there are no conflicts. Under ADC Settings, for ScanConvMode, it only has "Disable" in the drop-down list. Why is this? Another...

Issue when using CubeMX with Atolli

Hi,I am setting the Nucleo-H743ZI board with STM32 CumbeMX and when trying to compile the code with Atolli I am getting ..\Drivers\CMSIS\DSP\Source\BasicMathFunctions\arm_dot_prod_q7.c:29:22: fatal error: arm_math.h: No such file or directoryI see ot...

SZoha by Associate II
  • 853 Views
  • 0 replies
  • 0 kudos

Resolved! I2S master transfer signal is something wrong

My environment is Nucleo-F446RE with STM32CubeMX 5.1 / TrueSTUDIO 9.3.​I created an I2S master transmit test program. [Full project archive is here]Transmission Mode / Mode Master TransmitCommunication Standard / LSB First(Right Justified)Data and Fr...

0690X0000088EAcQAM.png
Tank2005 by Associate II
  • 1737 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.