STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! STM32Cube_FW_H7_V1.4 when?

Hello,is it possible to know when will the 1.4 software version of STM32CubeH7 be released?Thanks in advance.

akosodry by Associate II
  • 2265 Views
  • 4 replies
  • 0 kudos

Logic inversion for CAN NART/AutoTransmission

I am using an STM32F4xx processor. I just worked through and tracked down a logic inversion between CubeMX and the HAL implementation, that does not show up in any of my searches. It looks like it got introduced when the CAN libraries were upgraded...

GSpri by Associate
  • 1266 Views
  • 1 replies
  • 1 kudos

STM32F4Disco + VCP + Windows10 issue: error code 10

Hi all,I want to handle STM32F407 Disco via VCP. In the first case, i tried to configure UART but when i connect my USB TTL converter to my PC: it informs me that VCP error ''This device cannot start(code 10)''.I thought that the probem is related ...

0690X0000088qxcQAA.png 0690X0000088qxSQAQ.png
mmed by Associate III
  • 2556 Views
  • 3 replies
  • 0 kudos

STM32L412RBT6, CubeMX code for USB FS MSC doesn't work.

I have designed STM32L412RBT6 board with USB FS connection. With CubeMX 5.0.0 and L4 firmware package V1.13.0, I generated USB MSC project for TrueStudio. But, it doesn't work at all.PC couldn't recognize my MCU. For test, I changed the MCU to STM32...

taz1000 by Associate III
  • 3491 Views
  • 8 replies
  • 0 kudos

Board configurations in a single CubeMX / Truestudio project?

Hi there, I have been developing a CubeMX generated project in TrueStudio for the STM32H7 EVAL board.I would like to get the same project running on the H7 Nucleo board, and then eventually on my own hardware. I'd like to keep configurations for all ...

Mttjcksn by Associate III
  • 1217 Views
  • 2 replies
  • 0 kudos

STM32CubeMX 5.0.0 won't start on Ubuntu 18.04

Hello,I downloaded the new CubeMX from the ST site, launched the installer (as the root user) and started the application. It can't start, it hangs at startup. Here are the logs obtained at app startup:chdir /home/kacper/STM32CubeMX/.current dir /hom...

KKowa by Associate
  • 2795 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.