2018-12-11 9:58 PM
The project was create in CubeMX of earlier verson 4.29.0 , and it can easily to generate code. But a couple of days earlier, I need to add a new pin to the project. So I added the pin configure in CubeMx of Verson 5.0.0. When I generate codes, tips above happens. So how to solve the problem.
2019-03-20 7:20 PM
Set an input pin and select that input pin.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.