2019-03-23 4:40 AM
Hi,
I have a problem with connecting my STM32 F4 Discovery to USB. I use Eclipse with CubeMX and I configured USB as Device_Only, VBUS_activate and the rest I left as default. I also set in USB_DEVICE the Class for FS IP "Communication Device Class (Virtual Com Port)". I did everything as in tutorials, like: https://www.youtube.com/watch?v=7oED-m34EKk
The program is compiling, I use ST-LINK to downloading programs to stm via SWD and it seems it has no errors. I have the STSW-STM32102 Virtual COM Port Driver installed. I use Windows 7.
The problem is when I plug in USB cable to stm nothing happens, it's not that the system can't recognize device as STM Virtual Port, it's just nothing appears. Can it be some hardware problem or something else?
I will be very thankful for any advice.
2019-03-24 1:23 PM
hi. i do the settings that has said in this film with stm32f407zgt board it work correctly , but please check this notes : in this film the HSE is 8M . your board must have a 8Mhz crystal , it is important .
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.