STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Lowercase Conversion Issue CubeMX v6.17.0

CubeMX copies the .s startup file from the template folder and renames it based on the selected MCU. However, the lowercase conversion generates different filenames on systems with different locale settings.For STM32H743IIK6, the generated filename d...

recepsah_0-1778222015189.png
recepsah by Associate II
  • 263 Views
  • 3 replies
  • 2 kudos

STM32F7 - Unable to Select I2S Mode for SAI1 in CubeMX

Hi: My goal is to perform full-duplex I2S using the STM32F722RET6 part. To achieve this using the pins available on the package it looks like I need to use SAI2 (sub-block B) as the master/TX and SAI1 (sub-block A) as a slave/RX synchronized to SIA2....

2026-04-22_11-27-27.jpg
Extra by Associate II
  • 462 Views
  • 7 replies
  • 1 kudos

[STM32H563] [STM32CubeMx] Unable to enable PTP

Hello,For one of my project, my goal is to use PTP to synchronise multiple STM32H563 to one host.However, when configuring the ETH Device, I can only enable RMII, as the "RMII_PTP_SYNCHRO" is greyed out.I've read the pop up that tells me to enable TI...

AMouton by Associate II
  • 542 Views
  • 5 replies
  • 3 kudos

CubeMX don't generate rightly for cube IDE. Linux.

I tried multiple times to generate code on Arch Linux with CubeMX version 6.17.0 and Import in CubeIDE version 2.1.1. I made a video with process. And I don't know why this not working. I tried last and previos version of packages for STM32F0. And I ...

Снимок экрана_20260502_233536.png Снимок экрана_20260502_233701.png
MrKimler by Associate
  • 335 Views
  • 1 replies
  • 1 kudos

Resolved! STM32C092GCU6: FDCAN interrupt handler name mismatch

Hello,   I may have found a bug related to the STM32C092GCU6 MCU and the FDCAN peripheral.   I created a new project and experienced issues with FDCAN reception: no RX messages were received, and the callback HAL_FDCAN_RxFifo0Callback() was never tri...

Vric by Associate
  • 325 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.