2026-05-07 11:34 PM - edited 2026-05-07 11:36 PM
CubeMX copies the .s startup file from the template folder and renames it based on the selected MCU. However, the lowercase conversion generates different filenames on systems with different locale settings.
For STM32H743IIK6, the generated filename differs depending on the system locale.
On Windows 11 with the English locale, CubeMX generates:
startup_stm32h743iikx.s
On Windows 11 with the Turkish locale, it generates:
startup_stm32h743ııkx.s
The issue is caused by locale-dependent lowercase conversion of the letter I.
2026-05-07 11:47 PM
Hello @recepsah
Is this conversion causing any build error or any problem with your generated project?
It would useful if you could provide all details about the issue that you are facing?
Thx
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-05-07 11:59 PM
Hello @Ghofrane GSOURI ,
We do not encounter any compilation errors. However, since we are using a source control system, this issue results in unnecessary file changes and repeated commits due to locale-dependent filename generation.
Recep
2026-05-08 2:26 AM
Hello @recepsah
I believe this is a low-impact, non-blocking limitation. A simple workaround is to use English as the system locale, which prevents locale-dependent filename differences during project generation and avoids unnecessary file renames in source control.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.