STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

cannot install cube in disk d.

While I am installing stm32cubemx v5.3 in my PC, and changing the installation path to somewhere in disk D. It is posted that: Invalid directory path. Please enter a directory path that meets the operation system's requirements.Only default intallati...

spica lai by Associate II
  • 1269 Views
  • 0 replies
  • 0 kudos

How to use external clock with STM32L011

I am trying to use an external 8MHz clock with the STM32L011. I generate the clock using the MCO output on a STM32Nucleo-L476 board, and connect it to a STM32Nucleo-L011 board on its PA0 pi (A0 on the Nucleo's CN4 connector). I used STM32CubeMX to ...

pgregson1 by Associate III
  • 2005 Views
  • 3 replies
  • 0 kudos

STM32CobeMx bug with STM32F407, FReeRTOS, FAT and USB

Hi,There is a bug in newest STMCubeMx.When you have a project with STM32F407VGT and using FreeRTOS V10.0.1 and CubeMX V3.5.0 with Keil V5. The USB Storage and FAT-Filesystem is configured then the Cube produces a syscall.c with function calls to osS...

Osto by Senior
  • 1344 Views
  • 2 replies
  • 0 kudos

How to install Firmware Package ?

There would be a training course for STM32G4 in our city on Oct.22, I was accepted and was asked to install 3 software:1.STM32CubeMX V5.2.12.STM32CubeG4 Firmware Package3.IAR EWARM V8.40.1I have installed the first one, while the second is more than ...

MQ by Associate II
  • 3749 Views
  • 3 replies
  • 0 kudos

STM32L4 toggle pin issue.

I am using STM32 for the first time. I have Atollic and STM32CubeMX installed. The controller I am using is STM32L475VG. I am trying to toggle the LED pin and am using HAL_GPIO_TogglePin to do it. But the compiler is throwing up an error 'undefined r...

ARai by Associate II
  • 1980 Views
  • 4 replies
  • 0 kudos

Start PWM with DMA (HAL_TIM_PWM_Start_DMA) results in Hardfault

Hello,I want to create a simple PWM with changing duty cycle. To do so, I have created a PWM with fixed frequency. With the DMA, I change pulses which will result in a modification of duty cycle.To create something clean, I have configured STM32CubeM...

0690X000006CyCKQA0.png 0690X000006CyCPQA0.png
Geo En by Associate III
  • 22482 Views
  • 10 replies
  • 0 kudos

STMCubeMX 5.3.0 USB mouse code not working

I have custom board with a STM32F446 processor I am trying to testusing cubeMX (v5.3.0) generated code for a USB human interface (mouse).Unfortunately, I have had very sporadic results with getting the computerto recognize it as a USB mouse. The comp...

0690X000009joLoQAI.png 0690X000009joLjQAI.png

STM32H745 dual core communication

Hello​Since the MCU is relatively new and there are few references related to it I would like to ask if you are familiar of and could recommend any application note/tutorial/examples which clearly explain communication between CM7 and CM4 cores, shar...

MMatu by Associate III
  • 1760 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.