STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! stm32cubemx

Posted on June 26, 2018 at 20:50Hello,I am using the STM32CubeMX application version 4.26.0 (see the attached files)There is no option for me to choose 'Copy all used libraries into the project folder'. The radio button was there but it grey out (di...

NUCLEO_F429ZI MCO2 is not working

I have a NUCLEO_F429ZI board, I try to use the MCO2 output 50Mhz clock, but this function doesn't work.Please refer to the attached project, the IDE is TrueStudio and code generator tool is STM32Cube 5.0.0.I'm not sure this is my boards fault or F429...

How to get working with freeRTOS + SDIO + FATFS

I have generated code using STM32Cubemx v.5.1 i have selected SDIO and FATFS and i want to use freeRTOS . so as soon as i enable freeRTOS my FATFS stops mounting performing operations. how to get working with both ?? any suggestion ??

CJagt by Associate II
  • 5902 Views
  • 15 replies
  • 1 kudos

Resolved! No Errors No Warnings but my LED is not blinking i have configured the correct GPIO pin also Still the LED is not blinking?

Hello ,The Micro Controller Iam Using is STM32h743ZI. an iam using ST link V2 programmer.I have Configured My GPIO pins ,Clock and i have generated the code the code got generated without any errors once the code gets generated i have added the fol...

MGane by Associate II
  • 8839 Views
  • 3 replies
  • 0 kudos

Resolved! stm32h7xx_hal_exti.h file does not exist in H7 package

Hi,I'm working with the STM32H750VBTx and I switched to the latest FW version package, STM32Cube FW_H7 V1.3.2.CubeMX generated the stm32f7xx_hal_conf.h file and a line was added to this file:#ifdef HAL_EXTI_MODULE_ENABLED #include "stm32f7xx_hal_ext...

ADion by Associate
  • 2053 Views
  • 1 replies
  • 0 kudos

TrueStudio support for STM32CubeMX + STM32H745I-DISCO?

Hi,I bought a STM32H745I-DISCO dev board because STM32CubeMX support was mentioned. However I find that if I choose that board within Board Selector, then later look at Toolchain/IDE options, TrueSTUDIO is greyed out for some reason. Is this a known...

0690X000009k9VpQAI.png
rbow021 by Associate
  • 922 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.