STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Problems with importing project into STM32CubeMx

I have a nucleo-f103rb, and I downloaded the STM32Cube_FW_F1_V1.8.0 to try some examples. The Import function is not available in the software, and in case i try to load a project, I should have .ioc files which I do not in the STM32Cube_FW_F1_V1.8.0...

0690X00000AtO9vQAF.jpg

STM32CubeMX Memory Leak Windows

Recently I've found that whilst I was developing, Google Chrome would all of a sudden just crash with a memory error. I look over to task manager and realise that the CubeMX software which I was using to develop my Nucleo F303K8 (not a massive proces...

0690X00000AAQqWQAX.png

Resolved! STM32CubeMX FreeRTOS 10.2 Support

Hi,I would like to know, when STM32CubeMX will support FreeRTOS 10.2.BTW: Is there any roadmap or plan where we can look it up?Best regards

CubeMX CANFD problems with stm32H747

Dear all,the more I dig into the CANFD programming the more question marks I have concerning the CubeMX functionality.For instance you can select CANFD1 and CubeMX is proposing to use the pin PH14. However, according to DS12931 Rev 1 this pin is very...

mkrug by Associate III
  • 1664 Views
  • 4 replies
  • 0 kudos

Output Compare - Changing pulse

I am trying to generate pulses using output compare mode for my stepper motor on my board STM32f103C8T6 and STM32F401CCU6 on various timers. For some reason I am not able to change the period i want the signal to toggle at i.esConfigOC.PulseHere is...

0690X00000AtGddQAF.png 0690X00000AtGdnQAF.png
Safi N by Associate II
  • 1512 Views
  • 2 replies
  • 0 kudos

Set up a general purpose timer and verify its operation.

I have a new NUCLEO-H743ZI2 board and STM32CubeIDE.I've made a Blinky project and seen it work - via led and debugger.I'd like to configure a timer - using MX gui or not - and see it working in the debugger.I tried this...I created a new STM32 projec...

0690X00000At9kXQAR.png 0690X00000At9kSQAR.png 0690X00000At9khQAB.png 0690X00000At9kcQAB.png
RonH by Associate II
  • 3581 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.