STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Hi Guys I am using the DMA with uart and get some problem.

i using the cubmx and generate the code. I add the code in main function below ,(sur_dma_data[100] is arry and uint16_t size send i defined them before). but it is dose not work. can not see the any data from serilas port of my board . i check d...

kevin xu by Associate II
  • 2837 Views
  • 5 replies
  • 0 kudos

Resolved! BUG: CubeMX/CubeIDE does not initialize TIM20.TRGO2 on STM32G474.

The configuration for the Timer 20 TRGO2 setting is not included in the generated source code. I verified using "git diff" that when changing the setting the only modified file is the .ioc.I'm using the low level library for this timer. I haven't ver...

Herm by Associate III
  • 1357 Views
  • 1 replies
  • 0 kudos

STM32L552E-EV and STM32Cube_FW_L5_V1.1.0

Hello,I have a STM32L552E Evaluation Board, and I see that the Examples and Applications folders have projects for IAR, KEIL and CubeIDE. Previusly I used System Workbench for STM32, so I installed CubeIDE and I tried to run and debug some code in th...

Why Nucleo L053R8 crashes after 7~11 minutes of execution?

I'm using STM32CubeMX 5.2.0MCU: STM32L053R8TxFirmware: STM32Cube FW_L0 V1.11.2Toolchain/IDE: MDK-ARM V5Tested with 3 different boards, even with a default code (as generated by CubeMX) in debug mode, and also with a simple UART transmitter program (t...

elyes by Associate
  • 2265 Views
  • 4 replies
  • 0 kudos

Hardware Reset Affecting Input Capture Direct?

Hi,I have come across an unusal problem and I can't seem to figure out.I am using an RC transmitter to send signals to a receiver that is hooked up to an STM32F411VE board. I am reading the receiver signal using input capture direct mode (timer 2, ch...

0690X00000BwM9yQAF.png
GEvan.1 by Associate
  • 1343 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.