2020-01-23 2:30 AM
The configuration for the Timer 20 TRGO2 setting is not included in the generated source code. I verified using "git diff" that when changing the setting the only modified file is the .ioc.
I'm using the low level library for this timer. I haven't verifed if it happens with HAL as well.
CubeIDE:
Version: 1.2.1
Build: 5190_20200115_1224 (UTC)
STM32CubeG4 Firmware Package V1.1.0 / 28-June-2019
Solved! Go to Solution.
2020-01-23 5:35 AM
Hello @Herm ,
Thanks for your feedback, issue appears only with LL, it works fine with HAL.
It will be fixed in the next release.
Best Regards,
Khouloud
2020-01-23 5:35 AM
Hello @Herm ,
Thanks for your feedback, issue appears only with LL, it works fine with HAL.
It will be fixed in the next release.
Best Regards,
Khouloud
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.