STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

I am trying to build up a QSPI connection with the STM32H7 Nucleo Board (H743zi2). I generated the keil project(setup with CubeMX). Am measuring the CS and CLK with my oscilliscope & I cant see anything for QSPI clk more than 30MHz.

I have attached the main file.I am using nucleo 144 board and have setup the stm32 core for 480MHz(max), so max QSPI clock allowed is 240M/2=120MHz. But am not able to generate clock pulses if I set QSPI clock prescalar less than 8 (30MHz). I have tr...

Sk.2 by Associate II
  • 8016 Views
  • 9 replies
  • 0 kudos

How to connect 8 mems microphones to DFSM using 4 filters?

Hello! I am using a stm32f765 chip. I need to connect 8 microphones to the DFSDM, but there are only 4 filters in the chip and I cannot use the regular read mode from all 8 channels of the DFSDM. I found information that the dfsdm filter allows to re...

RTolm.1 by Associate
  • 1148 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeMX V4.24.0 code generation failure (bug report)

Posted on February 13, 2018 at 18:23ST: Bug report:I've just upgraded from CubeMX V4.23.0 to V4.24.0.Using this re a Nucleo 144 'F767 board, I'm finding that 'Menu => Project => Generate Code' works once, then fails thereafter in one of two ways:If '...

JB2500 by Associate III
  • 7626 Views
  • 9 replies
  • 0 kudos

FSMC PSRAM setup time

Hello, I am trying to test PSRAM memory on STM32L4R9-Discovery board (STM32L4R9AI), I still don't understand how to calculate the PSRAM setup time (address setup time), (data setup time), (data hold time) and (bus turn around time) could someone expl...

RS485 Pin Configuration Conflict

Trying to understand this warning when configuring pins for a stm32g071RB in CubeIDE. Enabling the RS485 Hardware Flow Control even with no other peripherals enabled causes the warning to flag to display. The explanation message does not explain much...

AChen.1 by Associate
  • 1021 Views
  • 0 replies
  • 0 kudos

Problem generating SW4STM32 Project on Windows 10

Hi,I use CubeMX to configure STM32 controllers (mostly STM32F746ZG for testing on a Nucleo-144 board, but also tried with other boards and single MCUs).Since I moved to Windows 10 64Bit, the generation of SW4STM32 projects does not work properly anym...

0690X00000Bw0n3QAB.jpg
SJaco.1 by Associate
  • 1453 Views
  • 1 replies
  • 1 kudos

Resolved! How install NFC5 package? not able to install

Hi, I am running STM32CubeMX 5.5.0 (newest)And downloaded the NFC5 2.0 expansion package from ST website, but when I try to install it in Cube it give me this error:How do I do to install it?I just got one NFC05A1 board to evaluate but got stuck in t...

0690X00000Bvy2eQAB.png

Errors when including "arm_math.h"

Micro-controller: STM32F407VGTCompiler: Keil V 5.28.0CMSIS Core Library: V 5.2.0DSP Library: V 1.6.0I need some help including the CMSIS DSP library in my project. I have included the CMSIS DSP library via Manage Run Time Environment, this links the ...

m_n by Associate
  • 4786 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.