STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Purpose of global interrupt (NVIC)

Hello! In STM32CubeMX I tried adding a input Compare direct mode to a timer for the STM32F767 part.It did not work until I checked the option under "NVIC Settings" to make the timer a global interrupt.Excuse the beginner question, but should not all ...

STM32G070RBT possible GPIO silicon bug?

Hello,We've been using STM32 for quite some time for multiple products.For a new design we would like to use the STM32G070RBT. However there is a strange behavior with GPIO PD0 and PD1:PD0 is configured as input with pullup enabled. PD1 is configured...

NFaut.1 by Associate II
  • 2603 Views
  • 5 replies
  • 0 kudos

Resolved! How to create a MDK-ARM Project with CUBEMX 5.6.0

Hello, I have recently switched computers and i have installed Keil IDE and CubeMX 5.6.0 onto the new PC, but when i create a project i get an error saying:"The code is successfully generated under........ but MDK-ARM V5.27 project generation have a ...

MikeP by Senior
  • 6515 Views
  • 7 replies
  • 0 kudos

Resolved! STM32H7 CAN FD configured as classic CAN 2.0

Hello, I am working with STM32H7. I need to configure the CAN FD to work as Classic CAN 2.0. I have found an example that configures the CAN FD as Classic CAN 2.0, but in the example the system clock is different from my system clock. I need to find...

VYoun by Associate III
  • 8262 Views
  • 7 replies
  • 0 kudos

Possible CubeMX Bug on Nucleo-L467RG : SD Card.

Hey guys,I'm pretty new to Stm32 controllers, but I might find a bug. Just want to report it, in case I am right.Im using Stm32 Workbench Eclipse, Stm32CubeMX and a Nucleo-L476RG.I tried to get a sd card working on my board. So I had a SD-Card onboar...

TNguy.9 by Associate II
  • 2904 Views
  • 7 replies
  • 0 kudos

BUG: CubeMX fails to initialize PLL2IS

STM32F437, STM32CubeIDE Version: 1.3.0Build: 5720_20200220_1053 (UTC)OS: Windows 10, v.10.0, x86_64 / win32Java version: 1.8.0_202IOC attached.In CubeMX-generated main.c, the Q register is not set:PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPH...

dac to comparator does not working interrupt

comparator does not interruptThis function handles TIM6, DAC1 and LPTIM1 interrupts (LPTIM1 interrupt through EXTI line 29). LL_EXTI_LINE_17 ? 17 ? 29 ? @file      : main.c LL_TIM_GenerateEvent_CC1(TIM6); LL_EXTI_EnableIT_0_31(LL_EXTI_LINE_17); LL_EX...

0693W000000VzD8QAK.jpg 0693W000000Vz0JQAS.jpg
Ecift.1 by Associate
  • 1353 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.