2020-04-12 7:30 AM
errors are...
C:\Users\user\AppData\Local\Temp\ccqZJPGM.s:295: Error: selected processor does not support `dsb 0xF' in Thumb mode
C:\Users\user\AppData\Local\Temp\ccqZJPGM.s:306: Error: selected processor does not support `isb 0xF' in Thumb mode
C:\Users\user\AppData\Local\Temp\ccqZJPGM.s:350: Error: selected processor does not support `dsb 0xF' in Thumb mode
C:\Users\user\AppData\Local\Temp\ccqZJPGM.s:371: Error: selected processor does not support `dsb 0xF' in Thumb mode
C:\Users\user\AppData\Local\Temp\ccqZJPGM.s:492: Error: selected processor does not support `dmb 0xF' in Thumb mode
C:\Users\user\AppData\Local\Temp\ccqZJPGM.s:555: Error: selected processor does not support `dsb 0xF' in Thumb mode
C:\Users\user\AppData\Local\Temp\ccqZJPGM.s:566: Error: selected processor does not support `isb 0xF' in Thumb mode
Drivers/STM32F4xx_HAL_Driver/Src/subdir.mk:63: recipe for target 'Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_cortex.o' failed
make: *** [Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_cortex.o] Error 1
I used this method to solve this problem(https://community.st.com/s/question/0D50X0000BsROqbSQG/compile-error-make-no-rule-to-make-target-rcs-needed-by-stop), but still can not be solved.
Can anyone help?
2020-04-12 6:11 PM
>I used this method to solve this problem
That link lists a couple of solutions and I don't see a definitive answer there, except perhaps the suggestion it's a Cube 5.3.0+ problem.
I suggest diff this Eclipse project file with another project with the same core that works, and if you find the likely missing/incorrect configuration stanza, fix it by hand and if it works, post the cause here and to the link, and add "Bug-report" to your topics (top-right icon).
2020-04-12 11:28 PM
Hi @Ryosh.1 , could you please share your ioc file ?
Thanks,
Khouloud
2020-04-12 11:41 PM
2020-04-24 5:08 AM
Hi @Ryosh.1 ,
It's strongly recommended to use CubeIDE as toolchain.
Please change the Toolchain used and you will get no error.
Best Regards,
Khouloud
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.