STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

DMAContinuousRequests option does not appear on STM32Cube when setting up ADC with DMA. Therefore I can't make ADC work with DMA.

I am using the NUCLEO-H743ZI board. And I'm using STM32CubeIDE Version: 1.3.1Build: 6291_20200406_0752 (UTC) It has 3 16-bit ADCs, none of the three seem to have DMAContinuousRequests in the ADC settings:The DMA Settings tab is populated as follows:I...

0693W000001cIOfQAM.png 0693W000001cIPJQA2.png
FG by Associate
  • 1927 Views
  • 1 replies
  • 1 kudos

[Bug] Heap and Stack size of 0x00

The Linker Script is not being updated, if a heap or stack size of 0x00 is being written in MX and a code is being generated. Also mx.scratch won't be deleted.I'm using STM32CubeIDE v 1.3.1 and tried it on the L011F4 and L452RE controllers.To set the...

AScha.381 by Associate II
  • 1692 Views
  • 2 replies
  • 0 kudos

NUCLEO-H745ZI-Q missing ram space in example project

Hi,I've just received new nucleo board, created new project for this board using cubeIDE and first thing i wanted to check is how the memories are split between cores and i'm a bit confused because i'm missing atleast 500k of RAM as it's not in linke...

gasda.1 by Associate II
  • 1559 Views
  • 2 replies
  • 0 kudos

Resolved! generation issue STM32CubeMX 5.6.1 - Timer init

When I generate for TIM9 input capture to measure a pulse width, CubeMX inserts correctly these two lines into the function MX_TIM9_Init: if (HAL_TIM_IC_Init(&htim9) != HAL_OK) { Error_Handler(); }Then in the stm32fxx_hal_msp.c file it inser...

STM32F103C8T6 ADC DMA Strage Readings

Hello everyone,I have a circuit that measures 6 adc inputs from various voltage readings. I've got 3x4 pcs 7 segment displays and 4 buttons on the circuit. Tim1 is working on 100uS to generate a 100us tick and display scans.the thing is when I left ...

e-zeki by Associate III
  • 3535 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.