STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Resolved! Using FreeRTOS with TrustZone in STM32CubeIDE - STM32L562

I have a development kit for the STM32L562, I'm trying to create a blinky-script that will use FreeRTOS to blink a led in the secure-world and the non-secure world simultaneously.Steps to reproduce:Install STM32CubeIDE 1.3.0New STM32 ProjectLook for ...

FHumb.1 by Associate II
  • 5535 Views
  • 10 replies
  • 0 kudos

Bug in CubeMX v 5.6.1 when selecting DMA for ADC1/2 and BDMA for ADC3 for STM32H753IITx? Is there a fix or have I done something wrong?

Generated code in main.c looks like this and lacks function name for the second block./**  * Enable DMA controller clock */static void MX_BDMA_Init(void) { /* DMA controller clock enable */ __HAL_RCC_BDMA_CLK_ENABLE(); /* DMA interrupt init */ /* BD...

DGrön.1 by Associate II
  • 1611 Views
  • 3 replies
  • 0 kudos

Resolved! PWM output generation from NUCLEO-F031K6 (MCU: STM32F031K6) is not working. Code is generated from STM32CubeMx.

I'm using NUCLEO-F031K6 (MCU: STM32F031K6) for PWM output generation (100Hz clock). Project is generated from STM32CubeMx v5.6.1. PA11 (TIM1_CH4) is used for PWM output. No clock pulses are seen. APB1 timer clock is 8MHz. ----------------------------...

S.Kamath by Associate III
  • 940 Views
  • 1 replies
  • 0 kudos

ARM CMSIS 5.7.0

I've been trying to download the CMSIS 5.7 update for almost a month now.But when I try to download and install the library every day, I get errors in the file in the attached screenshot.Every day I hope that you have noticed the problem or that some...

RMent.1 by Associate
  • 2050 Views
  • 4 replies
  • 0 kudos

trying to operate an external interrupt on stm32f031k6

Im trying to operate an external interrupt on my STM32F031K6, using STM32cube IDE. Ive been following a tutorial here https://simonmartin.ch/resources/stm32/dl/STM32%20Tutorial%2007%20-%20GPIO%20Interrupts%20(EXTI)%20using%20HAL%20(and%20FreeRTOS).pd...

deep_rune by Associate III
  • 1332 Views
  • 1 replies
  • 0 kudos

Change peripheral ( USART ) config ( CubeMX )

Hi, by following some video i am able to create a GUI ( ST32F469I-DISCO ) and get a complete CubeIDE project... I create the GUI by selecting the right application template for the TouchGFX project ( device ). Then i can generate the code. After th...

LFili.1 by Associate II
  • 3376 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.