2020-07-04 7:57 AM
I'm using NUCLEO-F031K6 (MCU: STM32F031K6) for PWM output generation (100Hz clock). Project is generated from STM32CubeMx v5.6.1.
PA11 (TIM1_CH4) is used for PWM output. No clock pulses are seen.
APB1 timer clock is 8MHz.
------------------------------------
Timer-1 settings:-
------------------------------------
Prescaler: 79
Counter Period: 999
Pulse: 500
Any clue?
GPIO toggle is working for the same pin, PA11
Solved! Go to Solution.
2020-07-04 8:38 AM
Read out and check/post the TIM1 and relevant GPIO registers content.
Make sure TIM1_BDTR.MOE is set.
JW
2020-07-04 8:38 AM
Read out and check/post the TIM1 and relevant GPIO registers content.
Make sure TIM1_BDTR.MOE is set.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.