STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Ipv6 self-assigned address (Stateless autoconfiguration)

I am using STM32f769Ni discovery board. I need to transfer the data from discovery board to another node via ethernet. Here i have to use the discovery board as client.Another node acting as server. I need to use the Ipv6 self-assigned address(statel...

KP.1132 by Associate II
  • 1407 Views
  • 1 replies
  • 0 kudos

Saving data to SD card

Hello everyone,In CubeMX 5.3.0 I have configured FATFS+DMA+SDMMC for a card running STM32F777VI. i've been trying to save some data into a .txt file.It works fine, but i can't write data to SD card as fast as I want. Requirement is to save 25 bytes ...

0693W000001tTBMQA2.png 0693W000001tTBbQAM.png
HChau.2 by Associate
  • 1701 Views
  • 2 replies
  • 0 kudos

How to import CMSIS DSP library without using CubeMX?

Hello everyone. I'm trying to use some functions available in the CMSIS DSP Library.First I tried to add the library through CubeMX->Additional Software, but found a known bug reported here. According to this link, this bug should be fixed for the ne...

Ajudi.1 by Associate II
  • 2150 Views
  • 3 replies
  • 0 kudos

No updates for CubeMX?

CubeMx has not found any updates. Do they still arrive by autoupdate in Cube or should I search in GitHub?

LMI2 by Lead
  • 884 Views
  • 1 replies
  • 0 kudos

STM32G071KBU6N GPIO issue, IDE error.

Hello, I am quite new to G071 series, first attempt I collided with DMAMux, solved and it work like a charm.Project is simple, just read input value pack to two half word then dma transmit by SPI.Based on STM32G071KBU6N (UFQFN32) same bin bought in J...

0693W000001tA0UQAU.png 0693W000001tA13QAE.png

Does SD work with CubeMX 5.6.1? (STM32F411/STM32F412)?

I have found an old videohttps://www.youtube.com/watch?v=0NbBem8U80Ytelling CubeMX 4.24 and 4.23 had a bug with SDIO, 4 bit mode, DMA.It seems for them 4.21 worked.I am using newest CubeMX 5.6.1. When was bug fixed? I assume it was fixed also in vers...

STMCube DMA settings on QUADSPI for STM32F413ZH not working

HiI am using STM32CubeIDE 1.3.0 on a Linux host to set up a NUCLEO-F413ZH.I was setting up the QSPI port DMA. This does not allow you to click on the checkbox to increment memory.As a result, the generated code is wrong and the DMA address does not ...

CMann.2 by Associate
  • 1094 Views
  • 1 replies
  • 0 kudos

Resolved! What is MBEDTLS used for?

Mbed environment looks interesting, mainly because it supports many interesting peripheral chips. I see that there is a MbedTLS option in CubeMx. What is it, how should it be used. Why should I use it. Main.c looks the same as without the Mbed. PDFs ...

LMI2 by Lead
  • 3089 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.