2020-07-20 10:15 AM
Mbed environment looks interesting, mainly because it supports many interesting peripheral chips. I see that there is a MbedTLS option in CubeMx. What is it, how should it be used. Why should I use it. Main.c looks the same as without the Mbed. PDFs are nice but a few words are enough now.
Edit: Google tells me MbedTLS is for encryption. Not much use for me, I think.
Solved! Go to Solution.
2020-07-20 11:14 AM
TLS is the new SSH. It may be used alone, or as transport layer of other protocols built upon it, most prominently HTTPS.
JW
2020-07-20 11:14 AM
TLS is the new SSH. It may be used alone, or as transport layer of other protocols built upon it, most prominently HTTPS.
JW
2020-07-21 3:00 PM
Not the new SSH, but the new SSL. If we can call a name from year 1999 a new... :)
Mbed - a software platform and operating system (in a broader sense, not only kernel) from ARM.
Mbed TLS - cryptographic library, one of the Mbed platform components.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.