2020-07-21 6:33 PM
Hi
I am using STM32CubeIDE 1.3.0 on a Linux host to set up a NUCLEO-F413ZH.
I was setting up the QSPI port DMA. This does not allow you to click on the checkbox to increment memory.
As a result, the generated code is wrong and the DMA address does not increment, so the transfer gets hosed.
Hand editing the code to change the MemInc field from Disable to Enable fixes this.
- hdma_quadspi.Init.MemInc = DMA_MINC_DISABLE;
+ hdma_quadspi.Init.MemInc = DMA_MINC_ENABLE;
Once that is fixed it all works great!
2020-07-22 3:46 AM
Hello @CMann.2
Thanks for your feedback, this will be internally checked.
Best Regards,
Khouloud
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.