STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Resolved! STM32CubeMX Toolchains greyed out

I am using STM32CubeMX v6.0.1. I am designing for the chip STM32L552RET6. The problem is I want to output as a GPDSC file and the option is greyed out. If I select a different chip, I can select that toolchain no problem. How do I force the applicati...

RMcNa.1 by Associate
  • 2301 Views
  • 1 replies
  • 0 kudos

bug report for STM32CUBEMX 6.0

using stm32cubemx 6.0 to make a project for STM32F103RC TIM init.the configuration as follow pictures.the code be generated as a wrong as follow.stm32cubemx version 6.0STM32Cube_FW_F1_V1.8.0

0693W000003BZ7pQAG.png 0693W000003BZ7uQAG.png
Bruno Hu by Associate II
  • 3138 Views
  • 3 replies
  • 0 kudos

CubeMX 6.0.1 has a new bug with project setting

I posted previous for 6.0 that there was a bug where it would change your ProjectManager settings from 'Add necessary library files' to 'Copy only the necessary library files'. (https://community.st.com/s/question/0D53W00000DffOTSAZ/updating-from-cub...

0693W000003Ph3yQAC.png
JKaz.1 by Associate III
  • 1527 Views
  • 2 replies
  • 0 kudos

Resolved! [bug] Issue generating code for freeRTOS using CubeMX 6 (I think)

I think there is a bug in the new CubeMX 6.0 when generating code using freeRTOS. It may just be when migrating from an older CubeMX project to a newer one, I'm not sure.I updated a project that was built using CubeMX 5.3 to CubeMX 6 and rebuilt all ...

JKaz.1 by Associate III
  • 3452 Views
  • 6 replies
  • 0 kudos

Resolved! flash memory-STM32F103C8

 STM32F103C8 , with MXCUBE, MDK-ARM V5. I would like to know how to program to store the counter value in flash memory even in power failure. when power goes up automatically recall the counter value. Please support me to solve this. I am not fully a...

Sbhus.1 by Associate
  • 1262 Views
  • 1 replies
  • 0 kudos

CubeMX timer period value generated wrong

CubeMX generates weird number for timer period.I set the timer period to 0xffffffff in the GUI. That results in CubeMX setting:4.294967295E9for the period. That value is wrong. It should be just 4294967295.Is that a CubeMX bug?

STM32H743 HRTIM Clock Configuration Bug from Stm32 CubeMx

MCU Reference STM32H743XIHxFirmware Package Name and version: STM32CUME FW_H7 V1.7.0CubeMx Version 5.6.1Bug exists in stm32H743xx.h and/or stm32h7xx_hal_rcc_ex.cClock selection always compiles as Tim2_Ck even when Cpu_Ck is selected on the clock conf...

JDoug by Associate
  • 1491 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.