2020-04-13 10:59 PM
MCU Reference STM32H743XIHx
Firmware Package Name and version: STM32CUME FW_H7 V1.7.0
CubeMx Version 5.6.1
Bug exists in stm32H743xx.h and/or stm32h7xx_hal_rcc_ex.c
Clock selection always compiles as Tim2_Ck even when Cpu_Ck is selected on the clock configuration page.
This is due to stm32h7xx_hal_rcc_ex.c looking for a definition of HRTIM (see line 1580). stm32H743xx.h has a defition of HRTIM1 (line 2393).
I worked around for now with a #define HRTIM HRTIM1
Cheers
James
2020-05-08 1:44 AM
Hello @JDoug
Could you please explain more the scenario to check the issue.
Best regards,
Nesrine
2020-08-17 4:20 AM
Hi Nesrine,
When trying to configure the HRTIM from CubeMx, the clock source cannot be set to 'Cpu_Ck' from the Clock Configuration Page. via the HRTIM Clock Mux. The clock always defaults back to Tim2_Ck when generating code.
This seems to be because The HRTIM1 Clock Configuration section of the stm32H7xx_hal_rcc_ex.c is checking if HRTIM is defined (see snippet below).
//stm32H7xx_hal_rxx_ex.c Line 1474
#if defined(HRTIM)
/*------------------------------ HRTIM1 clock Configuration ----------------*/
if(((PeriphClkInit->PeriphClockSelection) & RCC_PERIPHCLK_HRTIM1) == RCC_PERIPHCLK_HRTIM1)
{
/* Check the parameters */
assert_param(IS_RCC_HRTIM1CLKSOURCE(PeriphClkInit->Hrtim1ClockSelection));
/* Configure the HRTIM1 clock source */
__HAL_RCC_HRTIM1_CONFIG(PeriphClkInit->Hrtim1ClockSelection);
}
#endif /*HRTIM*/This HRTIM definition is also tested later on:
//stm32H7xx_hal_rcc_ex.c line 1581
#if defined(HRTIM)
PeriphClkInit->PeriphClockSelection |= RCC_PERIPHCLK_HRTIM1;
#endif /* HRTIM */The HRTIM definition doesn't exist so this code doesn't get called correctly.
HRTIM1 however is defined in the device header files, e.g. stm32h750xx.h or stm32H743xx.h
//stm32H750xx.h line 2466
#define HRTIM1 ((HRTIM_TypeDef *) HRTIM1_BASE)
#define HRTIM1_TIMA ((HRTIM_Timerx_TypeDef *) HRTIM1_TIMA_BASE)
#define HRTIM1_TIMB ((HRTIM_Timerx_TypeDef *) HRTIM1_TIMB_BASE)
#define HRTIM1_TIMC ((HRTIM_Timerx_TypeDef *) HRTIM1_TIMC_BASE)
#define HRTIM1_TIMD ((HRTIM_Timerx_TypeDef *) HRTIM1_TIMD_BASE)
#define HRTIM1_TIME ((HRTIM_Timerx_TypeDef *) HRTIM1_TIME_BASE)
#define HRTIM1_COMMON ((HRTIM_Common_TypeDef *) HRTIM1_COMMON_BASE)I edited the device file to add a definition of HRTIM as below:
//stm32H750xx.h line 2466
#define HRTIM1 ((HRTIM_TypeDef *) HRTIM1_BASE)
#define HRTIM HRTIM1 //Hack to define HRTIM
#define HRTIM1_TIMA ((HRTIM_Timerx_TypeDef *) HRTIM1_TIMA_BASE)
#define HRTIM1_TIMB ((HRTIM_Timerx_TypeDef *) HRTIM1_TIMB_BASE)
#define HRTIM1_TIMC ((HRTIM_Timerx_TypeDef *) HRTIM1_TIMC_BASE)
#define HRTIM1_TIMD ((HRTIM_Timerx_TypeDef *) HRTIM1_TIMD_BASE)
#define HRTIM1_TIME ((HRTIM_Timerx_TypeDef *) HRTIM1_TIME_BASE)
#define HRTIM1_COMMON ((HRTIM_Common_TypeDef *) HRTIM1_COMMON_BASE)So I think the bug is in the stm32h7xx_hal_rcc_ex.c testing if HRTIM is defined in two locations, rather than testing if HRTIM1 is defined.
Unless I've done something silly? :D
Cheers,
James
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.