STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Hi, i'm a beginner and need some help. I bought a nucleo g474 Board and followed 2 startup how tos. Keil + Cubemx. When i produce the initialisation code i always get the error in the stm32g4xx_ll_fmc.c file Does anybody know what im doing wrong?

C:\Users\marti\AppData\Local\Arm\Packs\Keil\STM32G4xx_DFP\1.1.0\Drivers\STM32G4xx_HAL_Driver\Src\stm32g4xx_ll_fmc.c(176): error: #20: identifier "FMC_NORSRAM_TypeDef" is undefined HAL_StatusTypeDef FMC_NORSRAM_Init(FMC_NORSRAM_TypeDef *Device, FMC_NO...

Thomas1s by Associate II
  • 4623 Views
  • 9 replies
  • 0 kudos

Resolved! Use CubeMX STM32F103 Hard Fault exception??

Helloi'm using stm32f103rct.Use cubemx and just set RCC,and SYS(JTAG, Timebase Systick) compile with IAR and then download and debug press break.Hard fault exceptionhelp plz

0693W000004KMPxQAO.png
sjaey.1 by Associate II
  • 3884 Views
  • 9 replies
  • 0 kudos

Resolved! osMessagePut usages in UART ISR

Hi.I'm using STM32F746-DISCOVERY EVM with CubeIDE (v1.4.2)I'm trying to send uart rx char via osMessagePut API in uart ISR to other task which waits uart que.in uart isr callback, when I get rx char, I send rx byte via osMessagePut ().void HAL_UART_R...

0693W000004KKLoQAO.jpg
louiey by Associate II
  • 2100 Views
  • 2 replies
  • 0 kudos

Resolved! Why can't I get USB TX to work on my Nucleo board?

I am new to the ST world and have a Nucleo-H7A3ZI that I am testing with. I have STM32CubeIDE setup and have an LED toggling, so I am comfortable that I have the toolset configured properly.My next step was to send some characters over USB to the ho...

JMatu.1 by Associate II
  • 2298 Views
  • 6 replies
  • 0 kudos

USB Power switch on ERROR in CUBEMX software?

I have tried to get the USB FatFS MSC example for Nucleo 144 - STM32F429ZI working. After about 10 day I have succeeded, but I had to change the MX_DriverVbusFS in the usbh_platform.c file as follows:original code:void MX_DriverVbusFS(uint8_t state){...

HKnoe.1 by Associate
  • 1168 Views
  • 1 replies
  • 0 kudos

PVD code not generated by CubeIDE (but do in CubeMX)

Trying to to use PVD on F401 and CubeIDE but no relevant code is generated.I found on this forum code generated by CubeMx and it also works for me. Just copy and paste and corrected some minor differences like PVD_AVD_IRQn should be PVD_IRQnSo my ...

ICohe.1 by Associate III
  • 2032 Views
  • 2 replies
  • 0 kudos

When I add TIM4 with interrupts in the .ioc file, using the tool, it refuses to update the clock configuration to show that TIM4, and the timer does not perform normally

I add TIM4, with prescaler of 63 and period of 9, and enable the interrupt. The ISR should trigger each 1 msec. It does not, it triggers about every 1.3 msec. When I look in the SystemClock_Config function it has the following unexpected behavior, i...

CLee.0 by Associate III
  • 1640 Views
  • 1 replies
  • 0 kudos

Why did ST remove support for IAR EWARM V6 in MXcube 5 ?

So I said yes to updating to MXcube V 5.x and now I cannot compile the code because it generates code that is only compatible with the latest IAR EWARM versions. I have 6.x and there are evidently features in the new IAR versions that keep me from m...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.