2020-06-17 7:31 AM
Trying to to use PVD on F401 and CubeIDE but no relevant code is generated.
I found on this forum code generated by CubeMx and it also works for me. Just copy and paste and corrected some minor differences like PVD_AVD_IRQn should be PVD_IRQn
So my question is: How do I make CubeIDE generating code for activating PVD ?
The only relevant Item I found in CubeIDE is PVD interrupt through EXTI line 16
Here is what CubeMX generated:
The following code was generated by CubeMX in stm32h7xx_hal_msp.c:
void HAL_MspInit(void)
{
/* USER CODE BEGIN MspInit 0 */
/* USER CODE END MspInit 0 */
PWR_PVDTypeDef sConfigPVD = {0};
__HAL_RCC_SYSCFG_CLK_ENABLE();
/* System interrupt init*/
/* PendSV_IRQn interrupt configuration */
HAL_NVIC_SetPriority(PendSV_IRQn, 15, 0);
/* Peripheral interrupt init */
/* PVD_AVD_IRQn interrupt configuration */
HAL_NVIC_SetPriority(PVD_AVD_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(PVD_AVD_IRQn);
/** PVD Configuration
*/
sConfigPVD.PVDLevel = PWR_PVDLEVEL_7;
sConfigPVD.Mode = PWR_PVD_MODE_IT_RISING;
HAL_PWR_ConfigPVD(&sConfigPVD);
/** Enable the PVD Output
*/
HAL_PWR_EnablePVD();
/* USER CODE BEGIN MspInit 1 */
/* USER CODE END MspInit 1 */
}To those which are totally clueless (like me) you have also to create the following function that will be called when PVD is activated:
void HAL_PWR_PVDCallback(void)
2020-10-26 2:50 AM
Hello @ICohe.1
Could you please share your ioc file to check with.
Best regards,
Nesrine
2020-10-26 3:37 AM
Attached is my ioc file as it is now. in CubeIDE 1.4.2
It is possible that at the time of my original post, I used another version.
It is 4 month ago and the project is running because I found a solution as I wrote. I haven't tested if the issue was corrected in the current version.
Anyway thanks for getting back to me and I hope others will benefit from it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.