2021-01-15 8:50 AM
Hello,
I'm porting code from STM32F072 to STM32F103. In F0 I had a option in CubeMX to invert UART Tx pin polarity and it worked very well. I do not have this option in F103's. Is there any way to invert polarity in this uC?
BR, Daniel
2021-01-15 9:56 AM
Not that I'm aware of, the F1 is very old, and a lot of lessons from that design were learned and applied to subsequent ones.
Perhaps you can make a soft UART output with a TIM, and/or GPIO+DMA ? Or SPI
2021-05-23 3:51 AM
Hey,
so I'm getting back to work with this project and I have found software serial library on github, link below:
https://github.com/liyanboy74/soft-uart
This code look very elegant and simple. I will implement it today. This library has no option to invert Tx signal, but I think this has to be accomplished by setting the inverted state at idle time, and just adding NOT in SoftUartGpioWritePin funcion? Am I right?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.