STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Resolved! STM32F407 Virtual com port error 43

Hello, I use STM32F407 and I wanna config virtual com port on my board using CubeMX,but I always get error 43, I saw many topics, my stack size is 0x4000 and heap size is 0x2000.I tried to change max packet size, reinstall stm32 vcp drivers, but noth...

qqAnton by Senior
  • 3053 Views
  • 5 replies
  • 0 kudos

Resolved! CubeIDEMX doesnt' enable RCC bit?

I used STMCubeIDE to generate the following code...It is for Timer16 to count up and generate an interrupt after 100ms. Can someone tell me why the code did not set up __HAL_RCC_TIMx_CLK_ENABLE()?When I use the IDE to generate GPIO stuff it automat...

SWenn.1 by Senior III
  • 1396 Views
  • 2 replies
  • 0 kudos

Resolved! CubeMx RCC_ClockConfig fails

Hello,We have been using STCubeMx(v6.2.1) to generate our system initialization code. We started a new project for an stm32H7A3xx MCU.But with the auto-generated code, it fails on the HAL_RCC_ClockConfig->HAL_InitTick->HAL_SYSTICK_Config.We tried dif...

Aterrades by Associate II
  • 5548 Views
  • 6 replies
  • 0 kudos

Resolved! Sending more than 8 bits through SPI using HAL

Hello! I need to send/receive a 16 bits data to an external ADC, but I realized that SPI HAL functions just support 8 bits buffers. How can I send more than 8 bits? Even DMA function all work with 8 bits. In CubeMX I set the word length as 16.

Kolab by Senior
  • 4170 Views
  • 6 replies
  • 0 kudos

CubeMX Error: "NOT A VALID IOC"

Hi,I have installed STM32CubeMX on my laptop.The installation was successful.But when I try to create a project it says "Not a Valid ioc". I have tried the following steps but still the result was same:1) I forced uninstalled the software STMCubeMX.2...

0693W00000Bam6NQAR.png
RPari.3 by Associate II
  • 5470 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.