STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

CubeMX LwIP initial Ip problem

Hi, I kindly need your help. I have a STM32F769 and TCP server application . I am using LWIP stack . In my application server is arm and PC is client. When client tries to send something to arm, arm binds client’s ip address. So the connection is ok ...

nur by Associate II
  • 2174 Views
  • 4 replies
  • 0 kudos

Resolved! STM32CubeMX 6.3.0 BUG?

main.c generated by STM32CubeMX 6.3.0Line 23#include "usb_device.h"#include "usb_device.h" Are duplicated.Then MX_RTC_Init () is missing HAL_RTCEx_SetWakeUpTimer_IT ().

tsuna by Associate II
  • 1412 Views
  • 1 replies
  • 0 kudos

Good starting point for VCP module (FT232 replacement)

I just ordered a PCBA with FT232RL as USB-VCP bridge and found that these things are bulky, expensive and out of stock mostly. So why not design a USB-serial (eg. 3.3 V 9600 bd) bridge using any STM32?I am aware that CubeMX supports USB/VCP so this i...

MMMartin by Associate II
  • 2598 Views
  • 5 replies
  • 0 kudos

Devicetree generation for MCU

Hi,Zephyr OS use device tree to describe hardware layer on MCU. Is there anyway I can generate device tree from STM32cubeMX configuration (ioc file) as we can do it for MPU ? Thanks,

FLapo.2 by Associate
  • 1199 Views
  • 0 replies
  • 1 kudos

What is the relationship between HAL_ and MX_ APIs?

CubeMX provides a host of MX_ functions for which I'm unable to find any documentation.I can instea find extensive HAL and LL API documentation.And these APIs overlap like MX_TIMxx_EnablePWM and HAL_TIM_PWM_InitThere is also a lot of MX_init code but...

CCarb.1 by Associate
  • 2449 Views
  • 4 replies
  • 0 kudos

nucleo board STM32CubeMX clock configuration nonsense

Hi,I'm trying to set up the HSI (16MHz) on a nucleo-f446ze board. The clock configuration GUI is kinda misleading I guess: default PLLMUX configuration is selecting HSE, but HSE oscillator is not present by default on the nucleosselecting HSI on PLLM...

0693W00000D0s07QAB.png 0693W00000D0s0HQAR.png
SCott.1 by Associate
  • 3482 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.