STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! How do I enable MDMA_IRQHandler using STM32CubeIDE?

Hello there.I've setup simple transfer from SRAM4 to FMC NE1 on my STM32H750 board using MDMA. Write transfer itself complites, however no MDMA callbacks is ever called. After some digging i've found out that HAL_MDMA_IRQHandler is never called. On t...

BStud.1 by Associate II
  • 2228 Views
  • 2 replies
  • 0 kudos

LPUART + BDMA TX on STM32H730

I am attempting to use CubeMX to generate the code necessary to do a very basic demo of TX DMA using the LPUART and the BDMA peripheral (which as I understand it handles DMA for the LPUART1 which I'm using).Based on my reading of the reference manual...

AAG.1 by Associate
  • 2129 Views
  • 1 replies
  • 0 kudos

Resolved! Read state of caps lock from keyboard

keyboard-pc-usb-stm32​Is it possible to read state of capslock on/off with stm?​ Using HAL and cubemx HID configuration.​I can send report. But how to receive report - status?​​​​

oeliks by Senior
  • 2981 Views
  • 3 replies
  • 0 kudos

How to enter low-power run mode?

Hi!I'm using a STM32L433V and have to deal with that whole energy-saving topic.My use-case is the following:I've to count and debounce pulses from an external sensor with an 78Ah battery for about 5 years without charging. The pulses do come with abo...

Resolved! Why can't i enable SDIO in CubeMX on NucleoL452RE(P) while it is possible on the corresponding spare MCU

Hi,I bought some NUCLEO-L452REP (wich include STM32L452RET6 MCU with an SMPS support) particulary because of its SDIO interface.But this interface is not available (not displayed) in CubeMX for the nucleo while it is available if I choose the spare M...

0693W00000GY3wtQAD.png 0693W00000GY3wAQAT.png 0693W00000GY3xrQAD.png
FSULE.1 by Associate II
  • 1659 Views
  • 2 replies
  • 0 kudos

Can't get RX callback interrupt to be triggered

I've followed this tutorial word by word and I'm not entirely sure why:1) Nothing is being written to that rx_buffer[]2) Why the void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) isn't being called/triggered as shown in the videoI'm also using ...

Conflict between 6.2.1 and 6.2.0 project

Step to reproduce:1) Generate a project in CubeMX v6.2.0 and save it2) Open and modify the 6.2.0 project with CubeMX v6.2.1 (no migration or wathever), save the project3) try to reopen the project with v6.2.0, these window will popup: I need to use t...

0693W00000BbETyQAN.jpg
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.