STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Fail to generate code with cubeMx 6.4

Hello,I'm generating code with CubeMx 6.4.0 with a command line.The generation ends with an error even if the files seems to be correctly generated. Here's the log and the ioc file.ThanksJulien

JulienD by Senior
  • 2289 Views
  • 4 replies
  • 0 kudos

Resolved! STM32H7 nucleo - DMA tab in cubeMX configuration of SDMMC

Posted on January 12, 2018 at 20:49Hello,I am trying to use SDMMC/SDIO with DMA + FATFS. When creating project on stm32f7, I can find and configure DMA streams for the sdmmc.I am working with cubeMX version 4.23.Screenshot from STM32F7 - DISCO cube ...

0690X00000609JbQAI.png 0690X00000609LqQAI.png

Resolved! STM32H743 (STM32H7) SDMMC DMA not configurable

Hello, I'm attempting to use the SDMMC with an SD card, and with DMA. However, when I use the STM32CubeMX IDE, there is no option to enable or use the DMA. Using: STM32CubeMX version 5.3.0Here's the configuration for SDMMC1 on the STM32H743And here i...

0690X00000AA4V8QAL.png 0690X00000AA4VIQA1.png
caleb by Associate III
  • 10936 Views
  • 13 replies
  • 2 kudos

Resolved! Method to reorder peripheral init functions? (DMA BUG)

Is there a way to reorder the peripheral initialization functions in the main.c auto code without opening the .ioc file? MX_DMA_Init() was getting called after MX_USART1_UART_Init() in my project, which was causing the DMA instance's registers to not...

ALars.2 by Associate II
  • 1635 Views
  • 2 replies
  • 0 kudos

Resolved! cubeMX 6.4 dialog box breaks command line build

HelloVersion 6.4.0 (and maybe some versions before) introduces an ugly dialog box when generating code. This dialog box breaks command line generation because it needs somebody to click.Can it be replaced by a warning in the logs?ThanksJulien

JulienD by Senior
  • 2189 Views
  • 1 replies
  • 0 kudos

STM32CubeIDE v1.8 generation error

/** * @brief GPIO Initialization Function * @param None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0};   /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOB_CLK_ENABLE(); __HAL_RCC_GPIOC_CLK_ENABL...

ivainc by Associate III
  • 2223 Views
  • 3 replies
  • 0 kudos

Incorrect code generation for PLL of F767

I want to use HSI, not external component to generate frequency. I generate code by CubeIDE only (pack 1.16.1), there is no my code. I only add define USE_FULL_ASSERT and implement void assert_failed. But CubeIDE's code fails on assert_param(IS_RCC_P...

0693W000008xivuQAA.png 0693W000008xiw4QAA.png

CubeIDE strange build behaviour

I know, it's not easy to get this answer this way. I have a working F446RE code with CubeMX generated base in CubeIDE. I use the LL drivers and just simple int and string variables, not any dynamic memory handling. In some cases if I insert a new cod...

Peterb by Associate
  • 2435 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.