2022-01-01 3:49 PM
/**
* @brief GPIO Initialization Function
* @param None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(RFSW_GPIO_Port, RFSW_Pin, GPIO_PIN_RESET);
/*Configure GPIO pin : RFSW_Pin */
GPIO_InitStruct.Pin = RFSW_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(RFSW_GPIO_Port, &GPIO_InitStruct);
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */Users cannot add any modification due to 'user' section is out of function.
2022-01-02 5:24 PM
Include your IOC file or include sufficient information to duplicate the issue. Your post is lacking detail.
2022-01-03 2:15 AM
2022-01-03 6:14 AM
I didn't open it, but if unicode characters are crashing CubeMX, perhaps don't use unicode characters and stick with UTF-8.
It does not appear that GCC supports unicode.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.