STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

How to receive data from host under the STM32 Mass Storage FS?

Hi all, I am newbie in this field.Using the STM32CubeMX V6.3 to create a virtual memory stick and working well under win7/10.Using the sample code I can easily to send data to host as followingfunction sendDataToHost(...){ USBD_MSC_BOT_HandleTypeDef ...

JLee.64 by Associate II
  • 1628 Views
  • 2 replies
  • 0 kudos

Resolved! Using ADC with DMA on H7 causes DMA transfer error

Hello,I am trying to use circular DMA to transfer data from ADC1 into a buffer using CubeMX-generated code to configure the ADC and DMA. The DMA stream encounters a transfer error on transferring the first item.The device is an STM32H743.Using a debu...

MMevo.1 by Associate II
  • 4771 Views
  • 3 replies
  • 0 kudos

Resolved! STM32G4 RX DMA not working

I have a Nucleo board https://www.st.com/en/evaluation-tools/nucleo-g491re.htmlI have configured USART1 on PC4 and PC5 in STM32CubeMX, with interrupts and RX DMAI can send but not receiveI was able to get it working on a discovery board before with t...

STm32H745 M4 Clock limitation problem

Hi! I am working with the dual core STM32H745 nucleo board, currently on the M4 core.I am having trouble with configuring my wanted system clock frequency.I want the clock to be 200 MHz and accordingally i try to set it in the CubeMX clock config int...

0693W00000GYfaCQAT.png 0693W00000GYfdQQAT.png
yuri CH by Senior
  • 5354 Views
  • 13 replies
  • 0 kudos

Problem in CubeMX 6.4.0 with correct ADC settings

CubeMX 6.4.0 shows an invalid setting for ADC Continuous Conversion Mode.But this entry has to be disabled in this configuration for correct operation (one ADC channel is triggered by timer). It was also no problem in earlier CubeMX versions.@STM: Ca...

0693W00000HqSUaQAN.png
SStor by Senior
  • 1237 Views
  • 1 replies
  • 0 kudos

Resolved! I want to read / write NORFLASH that is externally connected to H723.

H723ZGT6 Nucleo-144CubeMX 6.3.0[ data sheet ]   H723: DS13313 Rev2[NOR Flash]   S25FL256L[Reference manual]   H723: RM0488 Rev2   S25FL256L: 002-00124 Rev. * HI am currently using H723 to create a project to read and write NORFLASH.However, the read ...

june by Associate III
  • 5398 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.