STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

BUG: CubeMX enables unused channel on dual-channel DAC

I configure STM32F767I(G-I)Tx via CubeMX. I enabled ADC_IN4 and DAC_OUT2 on dual-channel DAC.ADC_IN4 shares pin with DAC_OUT1. Even though DAC_OUT1 was not enabled in CubeMX I can see it applies voltage on the pin breaking ADC reading,This can be sol...

EHabi.1 by Associate
  • 2021 Views
  • 3 replies
  • 0 kudos

Resolved! Missing option in CubeMX for battery charging on STM32H730

In CubeMX ther is missing optines to select charging of the battery and the seceltion of charging resistor 1.5K or 5KI would expect it to be under "System Core" -> RCC as it should go into resig PWR_CR3 So for my system I have to duck in "main.c" HAL...

MRick.2 by Associate II
  • 3365 Views
  • 4 replies
  • 0 kudos

Resolved! Mass Storage Mode Receive Data From Host Fail Issue!

Hi All,I am working on a SCSI device read/write project.(Base on STM32CubeMX V6.4, Chip STM32F103)Now the windows can recognized this device as a pen driver and I can send data from Device to Host just like send data for read capacity.EXint8_t SCSI_P...

JLee.64 by Associate II
  • 1848 Views
  • 1 replies
  • 1 kudos

cubeMx End of life and open source

Hello,As far as I understood, stm32cubeMx will be end of life within some days / months / years.Can you provide timeline for it?And will it be released as open source project at this moment?ThanksJulien

JulienD by Senior
  • 2862 Views
  • 6 replies
  • 0 kudos

RTC in binary mode not working properly on STM32F746

Hi, I enabled RTC and calendar on a STM32F746 CubeMX project, and I can gather correct time informations when using BCD mode from the HAL_RTC_GetTime function, but when using the other option the "binary" mode, the informations I´m getting from GetTi...

EPHIL.1 by Associate II
  • 6167 Views
  • 5 replies
  • 0 kudos

Null pointer exception in Eclipse when opening IOC file

When running /opt/st/stm32cubeide_1.8.0/stm32cubeide under Ubuntu 20.04.3 LTS, I get the following NPE when double-clicking on the ioc file. Nothing happens at the UI level. I include the ioc file that makes the program crash in case it could be usef...

JLemi by Associate III
  • 1171 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.