STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! LWIP get HardFault_Handler after update on STM32CubeIDE v1.9.0!

Hi I moved a code that was working on STM32CubeIDE v1.8. But after update STM32CubeIDE v1.9 I am facing a new issue that I have never see before in STM32CubeIDE v1.8.0!I compared what was before and what we have now, see screen...Maybe to me need onl...

0693W00000Lw7D2QAJ.png
DK.7 by Senior
  • 4443 Views
  • 5 replies
  • 0 kudos

REENT compilation errors when upgrading CubeMX to 1.9.0

I upgraded my IDE to STM32IDE 1.9.0, and CubeMX to version 6.5.0 in order to develop on U5 familiy.I know the ST does not include freertos lib on CubeMX 6.5.0 any more.. but, since I allready working with it in other projects I would to keep it inste...

AA.10 by Associate III
  • 851 Views
  • 0 replies
  • 0 kudos

Externai interupts for I/O pin in OUTPUT

I'm using a board Nucleo Stm32F401RE on Stm32Cube 1.8.A simple question : I have cofigured, in MX, I/O pin PC5 as GPIO_EXT_INT5with interrupt in falling edge , pull_up enabled and NVIC[9:5] enabledRemember: in Nucleo board PA5 pin control in OUTPU...

LVara.1 by Associate II
  • 3761 Views
  • 7 replies
  • 0 kudos

ERR_MEM on lwip stack

Hello!I use MCU STM32F429ZIT6. My task is to receive data on UART for several hours and copy them to ethernet. My function to send data (I generated the code in the CubeMX program with no RTOS): void sendstring (char* buf_str) { tcp_sent (ss->pcb, tc...

DFomi.1 by Associate II
  • 3582 Views
  • 2 replies
  • 0 kudos

How to debug an USB-Connection?

Hello everyone,I am trying to expand the STM32Cube USB library which comes with the generated Code from STM32CubeMX. There are still some bugs in the Code but it is really hard to find them without appropriate debugging tools. The normal debugger can...

THe1 by Associate
  • 4874 Views
  • 4 replies
  • 0 kudos

CubeMX Forcing FreeRTOS to be included on STM32H7

This is really a CubeMX problem but didn't see a better forum to post to. I am trying to create a bare metal project with CubeMX for the STM32H7. I click File->New Project..., then select STM32H745/755 under the Line drop down on the MCU/MPU Select...

ttatakis by Associate III
  • 1789 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.