STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Unable to Import example .

  i am installed cube-MX for linux laptop version (6.17.0) and cube-IDE is (Version: 2.1.1) .For MX it shows option only generlic linux  so it is correct for linux laptop ? and for IDE is debian is fine . I refer you tube sessions for Example import ...

shreya_awati_1-1779432370928.png shreya_awati_2-1779432566427.png shreya_awati_3-1779432973798.png

Resolved! STM32U575ZIT6 and xcube-Freertos

IN short, it's not working. I normally use the standard (not x-cube) and L5 processors.  I'm going to the U5 processors for a larger project.  I've gone to Cube MX 6.17.0 and CubeMXIDE 2.1.1. Starting with a blank project, I configure the pins as usu...

STM32G474RB CubeMX ADC Clock Mux is swapped

Hello,the STM32G474RBTx CubeMX Clock Configuration ADC1_2 and ADC3_4_5 are swapped - the ADC1_2 Mux is actually referring to the ADC3_4_5 Mux, at least when it comes to the subsequent divider options in the respective ADC configurations.Setting ADC12...

janik by Associate II
  • 214 Views
  • 3 replies
  • 0 kudos

STM32H5 TIM12 no TRGO section in CubeMX

Hello EveryoneI am using CubeMX 6.17.0 and Embedded Software Package STM32H5 1.6.0:Is there a control missing to setup "Trigger Output (TRGO) Parameters?  In comparison to e.g. Tim15:   

JohVis71_0-1777452694901.png JohVis71_1-1777452714813.png
JohVis71 by Associate II
  • 309 Views
  • 4 replies
  • 0 kudos

Resolved! Wrong comment in generated code

I'm using STM32CubeMX 6.17.0 with NUCLEO-U575ZI-Q, it generated the following code:/* Initialize COM1 port (115200, 8 bits (7-bit data + 1 stop bit), no parity */ BspCOMInit.BaudRate = 115200; BspCOMInit.WordLength = COM_WORDLENGTH_8B; BspCOMInit.Sto...

nicolas by Senior II
  • 163 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.