STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1757 Views
  • 0 replies
  • 2 kudos

Resolved! Problem with new version STM32CubeIDE ver1.5.1 and STM32CubeMX ver6.1.1 (fatal error: usb_device.h: No such file or directory)

Before that there was STM32CubeIDE ver1.4.0 STM32CubeMX ver6.0.0 everything was fine.Installed STM32CubeIDE ver1.5.1 and STM32CubeMX ver6.1.1, there was an error when connecting USB_DEVICE.Tried creating a project from scratch with nothing but USB_DE...

0693W000007BX7KQAW.png
ADysh.1 by Associate II
  • 8708 Views
  • 10 replies
  • 1 kudos

Resolved! STM32CubeIDE 1.10.0 Migration Issue

Hi, I am experiencing issues migrating projects from STM32CubeIDE 1.9.0 to 1.10.0. After performing the migration, a number of custom project .c/.h files are deleted from the project and filesystem, and some are completely replaced, deleting /*USER ...

Interrupt callbacks is not working, v 6.6.0

I've followed st video lab: https://www.youtube.com/watch?v=urHGtvLYctkDebugging the code, the calback (e.g. HAL_UART_RxCpltCallback) is not called (breakpoint is set). I tried with the "Register Callback" Enabled and Disabled, but none is working. ...

ksale.1 by Senior II
  • 2323 Views
  • 3 replies
  • 0 kudos

I2C conflict with timer output

hello to everyone, i am using stm32f429zi to generate a pulse for a triac . It all function without a lcd display.when i write the code to init the display(via I2C) ,,, the display works very fine but i have a problem ... the output of timer1 doesnt ...

LFerr.7 by Associate II
  • 2199 Views
  • 2 replies
  • 0 kudos

Resolved! MX6.5.0 Pinout->List Pinout Compatible MCUs never finishes

It stops at 95% on two different machines, the Windows Task Manager runs the MX task at 95-100% up until 95% and then goes to 0 "forever". Windows 10 Pro 64bit, all service packs, Intel Core2 and i7, 12GB RAM. Processors used in IOC file STM32F767BIT...

0693W00000NqsYIQAZ.jpg
GoEk by Associate III
  • 3854 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.