STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! I can not trust the MX plugin to generate the right code. I cannot get the serial port to work at all with the generated code. It used to work no problem.

First the GUI is all screwed up. When I look at USART2 It gives me the choices forGPIO output level,GPIO mode, GPIO Pull-up/Pull-downMaximum output speedUser Label,it is missing Fast Mode. I click down to USART1_TX and the list is different. It hasGP...

0693W00000NsptCQAR.png 0693W00000NspvDQAR.png
KiptonM by Lead
  • 4074 Views
  • 11 replies
  • 0 kudos

Resolved! Why does ST not publish a list of known problems with STM32CubeIDE and STM32CubeMX, and possible workarounds, until they are fixed?

I have spent hours trying to find bugs, and when I report them I am told they are "known problems". And the ST employee points to a number, that is internal to ST only. Companies publish Errata sheets all the time when the chip does not work as adver...

KiptonM by Lead
  • 1639 Views
  • 2 replies
  • 0 kudos

Competent using the Cube MX graphical config tool

Hi, I wonder if someone can explain how I can be more competent in using the CubeMX graphical tool for various peripheral configurations. Take for example, I am familiar with UART port hence the Cube MX GUI config tool for the UART is easier for me t...

STehA.1 by Associate II
  • 2351 Views
  • 4 replies
  • 0 kudos

Resolved! Missing code during Code Generation - STM32CubeIDE version 1.9.0

Hi, I am using the STM32CubeIDE version 1.9.0 Code Generator feature (via the CubeMX graphical interface) and wanted to generate the 96 MHz sample clock for the I2S codec. Unfortunately, I found that the code generated under sub "void SystemClock_Con...

STehA.1 by Associate II
  • 3439 Views
  • 3 replies
  • 0 kudos

CubeMX package migration causes main.c file deletion

I created and developed a project for more than 4 years, and changes in the project have always forced us to migrate to newer versions of CubeMX and also newer software packages. The project is for an STM32F407VGT6 microcontroller. The last stable ve...

APari.2 by Associate
  • 1546 Views
  • 2 replies
  • 0 kudos

NUCLEO-L073RZ I2C 주파수 문�?�

안녕하세요, ​NUCLEO L073RZ를 사용하고 있습니다. 해당 보드로 I2C 통신�?� 진행하려고 합니다.다만, 사용하는 슬레�?�브 센서가 130HZ입니다. CUBE MX�?서는 최소 단위가 1kHZ 입니다. 해당 보드로는 130Hz�?� 주파수로는 통신�?� 불가능 할까요? 문�?�드립니다. ​

Damdori by Associate II
  • 5592 Views
  • 6 replies
  • 0 kudos

Resolved! Possible problems in Cube MX Version 6.5.0 for STM32H742

Dear all,I am using Cube MX to generate a template code for my new project. In Advanced Settings page under project manager tab, Init sub-routines order is not correct and I also cannot fix it. DMA is used in ADC1 and it should initialize before than...

0693W00000Npm3WQAR.png 0693W00000Npm3HQAR.png 0693W00000Npm0IQAR.png
TA1 by Senior
  • 5178 Views
  • 9 replies
  • 0 kudos

Resolved! STM32CubeMX fails to install en.stm32cubef4_v1-27-0.zip

I just downloaded both STM32CubeMX (windows) and en.stm32cubef4_v1-27-0.zip.When I try to install the F4 package, it ask me for confirmation of license, checks license,churns mightly for a long while, and finally says "Problem during Unzip".I confirm...

0693W00000QKL8yQAH.png

(Cube)MX configurator compatible with Discovery SMT32H735G-DK? (Partly Disabled IO conflicts, Examples contain no .IOC, lwIP & RTOS creates code not compiling).

I am trying to do UDP on Discovery STM32H735G-DK.1)     MX Pinout configuration tool seems not compatible with the examples: if I open the example LwIP_UDP_Echo_Server in the configurator, LwIP remains disabled in the MX pin configurator.Q1: Is there...

0693W00000NsERLQA3.png 0693W00000NsERQQA3.png
Johi by Senior III
  • 3287 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.