STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Resolved! STM32CubeMX does not always update .project files

STM32CubeMX does not always update the .project files when code is regenerated on an STM32H7 project. This is especially true when moving a peripheral from one core to the other. For example, I generated a project with SPI1 and I2C4 in the M4 contex...

WLear by Associate III
  • 1882 Views
  • 2 replies
  • 0 kudos

(1) Which STM32F2 and (2) purchased where?

(1) Please tell me if I'm on the correct track here. I have an STM32F1 design (STM32F105RCT6TR) and a STM32CubeMX .ioc file that I used for pin-out assignment in the 64-LQFP package. This morning I created a new .ioc file for an STM32F2 (more speci...

HForr.1 by Associate II
  • 6498 Views
  • 12 replies
  • 0 kudos

Resolved! CubeMX: Project generation have problem

MCU reference : STM32F429ZITxFW package name : STM32Cube FW_F4 V1.25.0MDK ARM(Keil) version : 5.30STM32CubeMX verision : 5.6.1​at that time, i want to create code but i can not. just [the code is successfully generated under ~~ .but MDK ARM V4 projec...

CMOON.1 by Associate II
  • 10775 Views
  • 15 replies
  • 1 kudos

Need 3 cost effective USB ports

Currently, my custom PCB with STM32F105RCT6TR based on STM32CubeMX software has a single usb DEVICE port connecting to a display head that must play the role of USB Host. Note I'm also using dual CAN plus 5 analog inputs.Now I need to connect TWO usb...

HForr.1 by Associate II
  • 7056 Views
  • 15 replies
  • 0 kudos

Resolved! Servo not working with STM32F767Zi

I'm trying to control a Servo motor (MG90S) using the STM32F767Zi by leveraging the TIM2 Channel 1 (PA0). The Servo requires a 50Hz frequency (20ms) signal. The APB1 bus gives TIM2 timer port 108MHz frequency. The Servo is powered through a 5V port t...

0693W00000QMbXyQAL.png
VNaid.2 by Associate
  • 2093 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.