STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1756 Views
  • 0 replies
  • 2 kudos

Can't ping H743ii + dp83869. CubeIDE 1.9.0, CubeMX, HAL, noOS, MII, LwIP. But on devbords Nucleo_h745zi2 + PD83869EVM code works fine.

Get a problem with ETH on H7 family. On my dev-board-stand-with-ugly-wired-beard (pic.1) Nucleo_h743zi2+ Dp83869EVM my project works fine. Project (.ioc in attach) generated by CubeIDE, with some adds:1) MPU:/* Disables the MPU */ HAL_MPU_Disable(...

Alex.E by Associate
  • 1702 Views
  • 1 replies
  • 0 kudos

Hello, I would like to know if i can delete the following functions : MX_SDMMC1_SD_Init(); MX_USB_Device_Init(); MX_USBPD_Init(); USBPD_DPM_Run();

After selecting the STM32L55E-EV evaluation board I have these default settings. On the other hand when I am in DEBUG mode these functions block me to debug the program.I just need the starting program to work with the I2S interface. Thank you for yo...

0693W00000Suaa4QAB.png
DYann.1 by Senior II
  • 1921 Views
  • 4 replies
  • 0 kudos

Resolved! ADC frequency not working as expected

I am using NUCLEO-STM32F446re board. It runs at 180MHz SYSCLK and ADC uses APB2CLK that can run at a maximum frequency of 90MHz. I am using STM32CubeIDE and the clock configuration looks as follows:My ADC setup looks as follows:My DMA setup: Just bef...

0693W00000SuQkEQAV.jpg 0693W00000SuQkJQAV.jpg 0693W00000SuQkOQAV.jpg
MRABA.1 by Associate II
  • 3826 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.